MCUXpresso SDK Documentation

MCUXpresso Software Development Kit (SDK)#

The MCUXpresso SDK is a comprehensive software enablement package designed to simplify and accelerate application development with Arm® Cortex®-M based devices from NXP, including its general purpose, crossover and wireless-enabled MCUs. It includes production-grade software with integrated enabling software technologies (stacks and middleware), reference examples, and more.

High-Level Block Diagram

Features#

Comprehensive Driver Library#

  • Flexible peripheral drivers for rapid development

  • Optimized for performance and code size

RTOS Integration#

  • FreeRTOS support with optimized configurations

  • Real-time application frameworks

  • Task management and scheduling examples

Middleware Components#

  • Connectivity stacks (USB, Ethernet, wireless, communication protocols)

  • AI inference engines and neural network libraries

  • Audio processing and voice recognition libraries

  • Security frameworks and cryptographic libraries

  • Graphics and user interface components

  • Motor control and real-time control libraries

  • File systems and storage solutions

  • Partner middleware can be added using CMake and west manifests

Extensive Examples#

  • Basic peripheral use cases to full technology demonstrations

  • Board-specific reference implementations

  • Out-of-box Demo Applications

  • Middleware component examples and integrations

Distribution Formats#

MCUXpresso SDK is available in two main formats:

GitHub Repository SDK#

Git-based distribution hosted on GitHub for modular development, continuous updates, and collaborative workflows. The SDK uses multiple repositories managed by the Zephyr west tool to provide flexible, component-based development. See Getting Started for setup instructions.

SDK Package#

Downloadable packages from SDK Builder for offline development. Starting with release 25.12.00, two package versions are available:

  • Classic SDK Package: Traditional board-specific packages with pre-configured IDE projects for MCUXpresso IDE, IAR, Keil, and other toolchains.

  • Repository-Layout SDK Package: Board-specific packages that maintain the same structure and build system as the GitHub Repository SDK, providing offline access to the repository-based development experience. Available when selecting the ARMGCC toolchain.

Note

From version 25.12.00 onward, selecting ARMGCC downloads the Repository-Layout version; all other toolchains remain in the Classic version.

Delivery and Release#

NXP integrates Coverity® Static Analysis and Black Duck Software Composition Analysis into the SDK development process to deliver secure, high-quality software.

  • Annual releases (June) for popular products, with Long Term Support (LTS) on GitHub — back-ported security (SVE/PSIRT) and severe bug fixes for two years.

  • Quarterly releases for NPI and recent products.

  • SBOMs provided for all GitHub SDK repositories.

Release

Release Name

Maintenance

LTS

26.06.00-LTS

2 years until June 2028

Quarterly

26.09.00

None, rebase to mainline

LTS

27.06.00-LTS

2 years until June 2029

Supported platforms are listed at mcuxpresso.nxp.com/sdk-versions.

Toolchain Support#

All driver examples and most application examples are provided for the following toolchains:

Toolchain

GitHub

Archive/Zip

Generated (west)

Getting Started

MCUXpresso IDE

❌

✅ eclipse

❌

Link

MCUXpresso for VS Code

✅

✅ CMake

N.A.

Link

IAR Embedded Workbench

✅

✅ EWARM

✅ EWARM

Link

Keil™ MDK-Arm

❌

✅ uVision

✅ uVision

Link

CLI GNU toolchain

✅

✅ CMake

N.A.

Link

Archive/Zip packages can be downloaded from SDK Builder or imported directly in VS Code and MCUXpresso IDE using the Import Wizard.

IAR and Keil projects can be generated from the GitHub SDK CMake examples using a west build command.

Repository Architecture#

The SDK uses a multi-repository structure on GitHub managed by the Zephyr West Tool, enabling:

  • Modular Organization: Drivers, RTOS, middleware, and examples in separate repositories

  • Customizable Manifests: Targeted setups for specific requirements

  • Selective Downloads: Include only needed components

  • Independent Updates: Component-level version control

  • Scalable Integration: Easy addition of new repository components

Support and Resources#

Community Support#

Documentation#

  • Comprehensive guides and API documentation online

Technical Support#

SDK Product Page#

Trainings#