Getting Started with Package# Table of Contents MCUXpresso SDK board support package folders Example application structure Locating example application source files Run a demo using MCUXpresso IDE Select the workspace location Build an example application Run an example application Run a demo application using IAR Build an example application Run an example application Run a demo using Keil® MDK/μVision Install CMSIS device pack Build an example application Run an example application Run a demo using ARMGCC / VSCODE MCUXpresso Config Tools MCUXpresso IDE New Project Wizard How to define IRQ handler in CPP files