MCUXpresso SDK Documentation

mbedtls_selftest_thread

mbedtls_selftest_thread#

Overview#

Purpose of this demo is to test valid multithread support for mbedTLS Hardware implementation. For that, two tasks performs in parallel cryptographic algorithm testing.

Prepare the Demo#

Connect a serial cable from the debug UART port of the target board to the PC. Start TeraTerm (http://ttssh2.osdn.jp) and make a connection to the virtual serial port.

  1. Start TeraTerm.

  2. New connection -> Serial.

  3. Set the appropriate COMx port (where x is port number) in port context menu. The number is provided by the operating system, and could be different from computer to computer. Select the COM number related to the virtual serial port. Confirm the selected port by clicking the “OK” button.

  4. Set following connection parameters in menu Setup -> Serial port. Baud rate: 115200 Data: 8 Parity: none Stop: 1 Flow control: none

  5. Confirm the selected parameters by clicking the “OK” button.

Running the demo#

When the demo runs successfully, the terminal will display similar information like the following:

mbedTLS version 2.28.1 fsys=260000000 Using following implementations: SHA: ELS PKC HW accelerated AES: ELS PKC HW accelerated AES GCM: ELS PKC HW accelerated DES: Software implementation Asymmetric cryptography: ELS PKC HW accelerated Create thread successfully Create thread successfully Task 1 is running

Task 2 is running

Task 1 is running

Task 2 is running

Task 1 is running

Task 1 is running

Task 2 is running

Task 1 is running

Task 2 is running

Task 1 is running

Task 1 is running

Task 2 is running

Task 1 is running

Task 2 is running

Task 1 is running

Task 1 is running

Task 2 is running

Task 1 is running

Task 2 is running

Task 1 is running

Task 1 is running

Task 2 is running

Task 1 is running

Supported Boards#