bee#
Overview#
This driver example should demonstrate how to setup BEE driver for on the fly decryption of data stored in QSPI memory region. The BEE is configuerd to decrypt all data starting from location 0x6000_0000 to 0x6001_0000 using AES ECB mode with user specified key. If the BEE_KEY_SEL fuse is programmed, then OTPMK key will be used instead. The example itself does not perform any data decryption operation over QSPI. It is used only as a BEE setup guide.
Supported Boards#
EVKB-IMXRT1050
Hardware requirements
Mini/micro USB cable
EVKB-IMXRT1050 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
BEE Example.
BEE was succesfully configured for reading from 0x60000000 to 0x60010000.
Example end.
MIMXRT1060-EVKB
Hardware requirements
Mini/micro USB cable
MIMXRT1060-EVKB board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
BEE Example.
BEE was succesfully configured for reading from 0x60000000 to 0x60010000.
Example end.
MIMXRT1060-EVKC
Hardware requirements
Mini/micro USB cable
MIMXRT1060-EVKC board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
BEE Example.
BEE was succesfully configured for reading from 0x60000000 to 0x60010000.
Example end.
EVK-MIMXRT1015
Hardware requirements
Mini/micro USB cable
EVK-MIMXRT1015 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
BEE Example.
BEE was succesfully configured for reading from 0x60000000 to 0x60010000.
Example end.
EVK-MIMXRT1020
Hardware requirements
Mini/micro USB cable
EVK-MIMXRT1020 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
BEE Example.
BEE was succesfully configured for reading from 0x60000000 to 0x60010000.
Example end.
MIMXRT1024-EVK
Hardware requirements
Mini/micro USB cable
MIMXRT1024-EVK board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
BEE Example.
BEE was succesfully configured for reading from 0x60000000 to 0x60010000.
Example end.
MIMXRT1040-EVK
Hardware requirements
Mini/micro USB cable
MIMXRT1040-EVK board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
BEE Example.
BEE was succesfully configured for reading from 0x60000000 to 0x60010000.
Example end.
EVK-MIMXRT1064
Hardware requirements
Mini/micro USB cable
EVK-MIMXRT1064 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
BEE Example.
BEE was succesfully configured for reading from 0x60000000 to 0x60010000.
Example end.