usb_pd_alt_mode_dp_host#
Overview#
This PD example is a simple demonstration based on the MCUXpresso SDK PD stack.
The application use the shield host board (om13790host) to implement the DisplayPort alternate mode.
It recognize attached video adapters (like “Type-C to DisplayPort” or “Type-C to HDMI”), and drive the adapter to work.
System Requirement#
Hardware requirements#
One Type-C shield host board
One 9V DC power supply
Type-C Cable
One hardware for a specific device, for example: one lpcxpresso54114 board
Personal Computer
Software requirements#
The project files are in:
<MCUXpresso_SDK_Install>/boards//usb_examples/usb_pd_alt_mode_dp_host/ / .
The
is Bare Metal or FreeRTOS OS.
Terminal tool.
Getting Started#
Hardware Settings#
For detailed instructions, see the appropriate board User’s Guide.
Please reference to the re-worked document for hardware settings. Please note that this case does not work with the SCH-32144 REV B of shield board because this verison of shield board uses PTN36502 and the I2C address of PTN36502 is 0x1A. To make it work, need to change the macro PD_PTN36502_SLAVE_ADDRESS from 0x12 to 0x1A.
Prepare the example#
For MCUXpresso, please reference to the MCUXpresso SDK USB Type-C PD Stack User’s Guide to make sure the SDK_DEBUGCONSOLE = 1 in project settings.
Download the program to the target board.
Power on shield host board then power on development board.
Run the example#
Download this program to the board.
Connect the video source (like: PC) to the MinDP port (J2).
Connect one video adapter (like: “Type-C to DisplayPort” or “Type-C to HDMI”) to the Type-C port (J1).
Connect one displayer to the adapter. For example: if the adapter is one “Type-C to DisplayPort” adapter, connect displayer to the adapter with one DisplayPort cable.
The video source (PC) will recognize the displayer and the displayer works.
The follow UGREEN USB-C to HDMI/VGA device has one issue. If keeping the device connected with shield host board, then reset mcu board, the UGREEN device doesn’t work.

Supported Boards#
MIMXRT1170-EVKB
FRDM-K22F
LPCXpresso55S69
EVK-MIMXRT1064
MIMXRT685-AUD-EVK
LPCXpresso55S16
MIMXRT1060-EVKB
MIMXRT1040-EVK
FRDM-MCXN947
LPCXpresso55S28
LPCXpresso55S36
MCX-N5XX-EVK
MIMXRT1060-EVKC
MIMXRT1160-EVK
MIMXRT1180-EVK
FRDM-K32L2A4S
MIMXRT700-EVK
FRDM-IMXRT700
EVK-MIMXRT595
EVK-MIMXRT685
MCX-N9XX-EVK
EVKB-IMXRT1050
EVK-MIMXRT1015
FRDM-MCXN236