ele_concurrent_access#
Overview#
This application provides a demonstration of how the SSS API may be used concurrently from two cores. It demonstrates how initialization may be done independently on both cores and how to safely prepare input data into S200-accessible memory if used from the NBU core.
Access serialization#
The S200 enclave supports receiving commands from multiple cores. For such cases, the S3MU driver functions for sending command messages and receiving response messages are wrapped in an S3MU-specific semaphore for command serialization between cores. This serialization is transparent to the driver’s user and the user does not need to manage this semaphore themselves.
However, on top of this there may be a need to serialize access to shared resources at the application layer, such as access to shared memory. Such a case is demonstrated by this application, in which the SEMA42 hardware semaphore is utilized.
Demo implementation components#
The application is divided into three main components:
the primary core
main.cfile,the secondary core
main.cfile,and the
common_definitions.hfile.
The individual core’s main.c implementation files are specific to the given
core. Definitions in the common_definitions.h file are the same for both
cores and are included in both core’s binaries separately. These definitions
were placed in a single file to reduce code duplication. The common definitions
may differ in small ways between cores; please see the note below or the code
itself for concrete examples.
NOTE#
This example showcases the requirement for buffers that are directly
accessed by the S200 to be placed into S200-accessible memory. Notably,
the S200 may only access Main-core memory and the shared memory between Main and
NBU core. Please note the code sections guarded by the
#if (defined(IS_RADIO_CORE) && (IS_RADIO_CORE > 0)) construct.
Building the application#
This shows example how to build application for kw47evk board with cm33_core0 core_id.
Change the -b <board> parameter based on board you want to build.
Change the -Dcore_id=<core_id> parameter based on board core you want to build.
For these parameters please see attribute boards: in primary/example.yml.
west build --sysbuild examples/secure-subsystem_examples/ele_concurrent_access/primary --toolchain armgcc --config debug -b kw47evk -Dcore_id=cm33_core0
Supported Boards#
KW47-EVK
Hardware requirements
Type-C USB cable
KW47-EVK Board
Personal Computer
Board settings
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Download the program to the target board.
The program may require to be loaded twice without a power-cycle in-between loads.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world multicore demo in the terminal window:
Secondary core started
Initialization of the S200 was first done by NBU core
ALL TASKS COMPLETED, CHECKING SUCCESS RATES :
Main core successfully completed 25 tasks out of 25
NBU core successfully completed 25 tasks out of 25
KW47-LOC
Hardware requirements
Micro USB cable
Personal Computer
KW47-LOC Board
Board settings
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Download the program to the target board.
The program may require to be loaded twice without a power-cycle in-between loads.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world multicore demo in the terminal window:
Secondary core started
Initialization of the S200 was first done by NBU core
ALL TASKS COMPLETED, CHECKING SUCCESS RATES :
Main core successfully completed 25 tasks out of 25
NBU core successfully completed 25 tasks out of 25
FRDM-MCXW72
Hardware requirements
Type-C USB cable
FRDM-MCXW72 Board
Personal Computer
Board settings
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Download the program to the target board.
The program may require to be loaded twice without a power-cycle in-between loads.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world multicore demo in the terminal window:
Secondary core started
Initialization of the S200 was first done by NBU core
ALL TASKS COMPLETED, CHECKING SUCCESS RATES :
Main core successfully completed 25 tasks out of 25
NBU core successfully completed 25 tasks out of 25
MCX-W72-EVK
Hardware requirements
Micro USB cable
Personal Computer
MCX-W72-EVK Board
Board settings
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Download the program to the target board.
The program may require to be loaded twice without a power-cycle in-between loads.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world multicore demo in the terminal window:
Secondary core started
Initialization of the S200 was first done by NBU core
ALL TASKS COMPLETED, CHECKING SUCCESS RATES :
Main core successfully completed 25 tasks out of 25
NBU core successfully completed 25 tasks out of 25
MCXW72-LOC
Hardware requirements
Micro USB cable
Personal Computer
MCXW72-LOC Board
Board settings
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Download the program to the target board.
The program may require to be loaded twice without a power-cycle in-between loads.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world multicore demo in the terminal window:
Secondary core started
Initialization of the S200 was first done by NBU core
ALL TASKS COMPLETED, CHECKING SUCCESS RATES :
Main core successfully completed 25 tasks out of 25
NBU core successfully completed 25 tasks out of 25