MCUXpresso SDK Documentation

ZPS_tsAplZdpMgmtDirectJoinRsp

ZPS_tsAplZdpMgmtDirectJoinRsp#

This structure is used to store Mgmt_Direct_Join_rsp message data - a response to a call to the function ZPS_eAplZdpMgmtDirectJoinRequest(). This response is issued by a remote node (Router or Coordinator) that has been requested to allow a particular device to join the network as a child of the node.

The ZPS_tsAplZdpMgmtDirectJoinRspstructure is detailed below.

typedef struct {
        uint8 u8Status;
} ZPS_tsAplZdpMgmtDirectJoinRsp;

where u8Statusis the return status for ZPS_eAplZdpMgmtDirectJoinRequest().

Parent topic:ZDP response structures