MCUXpresso SDK Documentation

trdc

trdc#

Overview#

The Multicore TRDC demo application demonstrates how to use TRDC on a multicore system to control the access policy of the memory block checker(MBC) and memory region checker(MRC), and how to configure the domain access control(DAC) for bus masters to access both secure and non-secure domains.

First, the primary core example uses 1 domain for secure access demo. The primary core which is secure first sets a MRC memory region and a MBC memory block to non-secure access only, then trys to access the memory which triggers the hardfault. In hardfault the access control is changed to secure access to resolve the error. Then, the primary core releases the secondary core from the reset. The secondary core example uses 2 domains, one is for secure access and the other is for non-secure access. By enabling different DAC configuration, different domain is used for the access control. The secure access process is the same as the primary core. In the non-secure access demo, the secondary core sets a MRC memory region and a MBC memory block to secure access only, and switch to the non-secure DAC configuration which force the core to be non-secure. Then trys to access the memory which triggers the hardfault. In hardfault certain flags stored in flash is set to let primary core know and update the configuration to non-secure access to resolve the error, because the TRDC is secure access only.

Supported Boards#

MIMXRT1180-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1180-EVK board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Compile the CM7 then the CM33 project to get the executable image.

  4. Follow the instruction of Bootable image generation section in getting started guide, to build and write the image using SPT tool. As HyperRAM is utilized as the communication memory between the two cores, it must be initialized before use. So when Build image in SPT tool, remember to set XMCD file which is HyperRAM initialization file. For the MIMXRT1180-EVK board, select boards/evkmimxrt1180/xmcd/hyperram_xmc_auto_detect.bin.

Running the demo

The log below shows the output of the trdc multicore demo in the terminal window, if the CM33 uses TRDC2 and CM7 uses TRDC1 by default:


TRDC example starts on primary core
In primary core example we use 1 domain for secure access only.
Set the selected MBC block to non-secure for domain that is secure access only
Core0 MBC violent access at address: 0x47400000
The MBC selected block is accessible for secure master now
Set the selected MRC region to non-secure for domain that is secure access only
Core0 MRC violent access at address: 0x 4100000
The MRC selected region is accessible for secure master now
TRDC example succeeds on primary core
Copy Secondary core image to address: 0x303c0000, size: 16208
Starting Secondary core.
The secondary core application has been started.

In secondary core demo we use 2 domains, one is for secure access only, and the other is for non-secure access only.
Secondary core secure access demo starts.
Set the selected MBC block to non-secure for domain that is secure access only
Core1 MBC violent access at address: 0x42000000
The MBC selected block is accessible for secure master now
Set the selected MRC region to non-secure for domain that is secure access only
Core1 MRC violent access at address: 0x60000000
The MRC selected region is accessible for secure master now
Secondary core non-secure access demo starts.
Set the selected MBC block to non-secure for domain that is secure access only
Set the selected MRC region to non-secure for domain that is secure access only
Core1 MBC violent access at address: 0x42000000
The MBC selected block is accessible for non-secure master now
Core1 MRC violent access at address: 0x60000000
The MRC selected region is accessible for non-secure master now
TRDC example succeeds on secondary core

Note: The “Copy Secondary core image to address…” log message is not displayed on the terminal window when MCUXpresso IDE is used. In case of MCUXpresso IDE the secondary core image is copied to the target memory during startup automatically.

FRDM-IMXRT1186
Hardware requirements
  • Type-C USB cable

  • FRDM-IMXRT1186 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Compile the CM7 then the CM33 project to get the binary trdc_cm33.bin.

  4. Follow the instruction of Bootable image generation section in getting started guide, to build and write the image using SPT tool. As HyperRAM is utilized as the communication memory between the two cores, it must be initialized before use. So when Build image in SPT tool, remember to set XMCD file which is HyperRAM initialization file. For the FRDM-IMXRT1186 board, select boards/frdmimxrt1186/xmcd/hyperram_xmc_auto_detect.bin.

Running the demo

The log below shows the output of the trdc multicore demo in the terminal window, if the CM33 uses TRDC2 and CM7 uses TRDC1 by default:


TRDC example starts on primary core
In primary core example we use 1 domain for secure access only.
Set the selected MBC block to non-secure for domain that is secure access only
Core0 MBC violent access at address: 0x47400000
The MBC selected block is accessible for secure master now
Set the selected MRC region to non-secure for domain that is secure access only
Core0 MRC violent access at address: 0x28100000
The MRC selected region is accessible for secure master now
TRDC example succeeds on primary core
Copy Secondary core image to address: 0x303c0000, size: 16208
Starting Secondary core.
The secondary core application has been started.

In secondary core demo we use 2 domains, one is for secure access only, and the other is for non-secure access only.
Secondary core secure access demo starts.
Set the selected MBC block to non-secure for domain that is secure access only
Core1 MBC violent access at address: 0x42000000
The MBC selected block is accessible for secure master now
Set the selected MRC region to non-secure for domain that is secure access only
Core1 MRC violent access at address: 0x60000000
The MRC selected region is accessible for secure master now
Secondary core non-secure access demo starts.
Set the selected MBC block to non-secure for domain that is secure access only
Set the selected MRC region to non-secure for domain that is secure access only
Core1 MBC violent access at address: 0x42000000
The MBC selected block is accessible for non-secure master now
Core1 MRC violent access at address: 0x60000000
The MRC selected region is accessible for non-secure master now
TRDC example succeeds on secondary core

Note: The “Copy Secondary core image to address…” log message is not displayed on the terminal window when MCUXpresso IDE is used. In case of MCUXpresso IDE the secondary core image is copied to the target memory during startup automatically.