gpio_led_output#
Overview#
The GPIO Example project is a demonstration program that uses the KSDK software to manipulate the general-purpose outputs. The example is supported by the set, clear, and toggle write-only registers for each port output data register. The example take turns to shine the LED.
Supported Boards#
EVK-MCIMX7ULP
Hardware requirements
Micro USB cable
MCIMX7ULP-EVK board
J-Link Debug Probe
5V power supply
Oscilloscope
Personal Computer
Board settings
No special settings are required.
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 5V power supply and J-Link Debug Probe to the board, switch SW1 to power on the board.
Connect a micro USB cable between the host PC and the J6 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, the following message is displayed in the terminal: If no LED is connected to the pin on the board, please use oscilloscope probe to touch the J11-1 then you can see the voltage change on the oscilloscope.
GPIO Driver example
The LED is blinking.
FRDM-K22F
Hardware requirements
Mini/micro USB cable
FRDM-K22F board
Personal Computer
Board settings
This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
And you will find the LED RED is taking turns to shine.
FRDM-K32L2A4S
Hardware requirements
Mini/micro USB cable
FRDM-K32L2A4S board
Personal Computer
Board settings
This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The led is taking turns to shine.
And you will find the LED RED is taking turns to shine.
FRDM-K32L2B
Hardware requirements
Mini/micro USB cable
FRDM-K32L2B board
Personal Computer
Board settings
This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
And you will find the LED RED is taking turns to shine.
FRDM-K32L3A6
Hardware requirements
Mini/micro USB cable
FRDM-K32L3A6 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
And you will find the LED RED is taking turns to shine.
FRDM-KE15Z
Hardware requirements
Micro USB cable
FRDM-KE15Z board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:: And you will find the LED RED is taking turns to shine.
GPIO Driver example
The LED is taking turns to shine
FRDM-KE16Z
Hardware requirements
Micro USB cable
FRDM-KE16Z board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:: And you will find the LED RED is taking turns to shine.
GPIO Driver example
The LED is taking turns to shine
FRDM-KE17Z
Hardware requirements
Micro USB cable
FRDM-KE17Z board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:: And you will find the LED RED is taking turns to shine.
GPIO Driver example
The LED is taking turns to shine
FRDM-KE17Z512
Hardware requirements
Micro USB cable
FRDM-KE17Z512 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:: And you will find the LED RED is taking turns to shine.
GPIO Driver example
The LED is taking turns to shine
FRDM-MCXA153
Hardware requirements
Type-C USB cable
FRDM-MCXA153 board
Personal Computer
Board settings
Prepare the Demo
Connect a Type-C USB cable between the host PC and the MCU-Link port(J15) on the target board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
And you will detect voltage toggle on J1_12 of board.
FRDM-MCXA156
Hardware requirements
Type-C USB cable
FRDM-MCXA156 board
Personal Computer
Board settings
Prepare the Demo
Connect a USB Type-C cable between the host PC and MB board J22.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
And you will detect voltage toggle on J4.P21 of MB board.
FRDM-MCXA346
Hardware requirements
Type-C USB cable
FRDM-MCXA346 board
Personal Computer
Board settings
Prepare the Demo
Connect a USB Type-C cable between the host PC and MB board J22.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
And you will detect voltage toggle on the RED LED.
FRDM-MCXC041
Hardware requirements
Type-C USB cable
FRDM-MCXC041 board
Personal Computer
Board settings
This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
9600 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
And you will find the LED RED is taking turns to shine.
FRDM-MCXC242
Hardware requirements
USB-C cable
FRDM-MCXC242 board
Personal Computer
Board settings
This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
And you will find the LED RED is taking turns to shine.
FRDM-MCXC444
Hardware requirements
Type-C USB cable
FRDM-MCXC444 board
Personal Computer
Board settings
This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo
Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
And you will find the LED RED is taking turns to shine.
FRDM-MCXE247
Hardware requirements
USB-C cable
FRDM-KMCXE247 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:: And you will find the LED RED is taking turns to shine.
GPIO Driver example
The LED is taking turns to shine
FRDM-MCXN236
Hardware requirements
Type-C USB cable
FRDM-MCXN236 Board
Personal Computer
Board settings
Prepare the Demo
Connect the type-c and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
If the EVK board is used then the red led will blink.
FRDM-MCXN947
Hardware requirements
Type-C USB cable
FRDM-MCXN947 Board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect the type-c and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
If the EVK board is used then the red led will blink.
FRDM-MCXN947T
Hardware requirements
Type-C USB cable
FRDM-MCXN947T Board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect the type-c and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
If the EVK board is used then the red led will blink.
FRDM-MCXW71
Hardware requirements
Type-C USB cable
FRDM-MCXW71 Board
Personal Computer
Board settings
Prepare the Demo
Connect a USB cable between the host PC and the FRDM board J10.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
And you will detect voltage toggle on J4.P31 of MB board. If the EVK board is used then the green led will blink.
MCX-W71-EVK
Hardware requirements
Type-C USB cable
MCX-W71-EVK Board
Personal Computer
Board settings
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
And you will detect voltage toggle on J4.P31 of MB board. If the EVK board is used then the green led will blink.
KW45B41Z-EVK
Hardware requirements
Mini/micro USB cable
KW45B41Z-EVK Board
Personal Computer
Board settings
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
And you will detect voltage toggle on J4.P31 of MB board. If the EVK board is used then the green led will blink.
KW47-EVK
Hardware requirements
Type-C USB cable
KW47-EVK Board
Personal Computer
Board settings
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
And you will detect voltage toggle on J4.P31 of MB board. If the EVK board is used then the green led will blink.
MCX-N5XX-EVK
Hardware requirements
Mini/micro USB cable
MCX-N5XX-EVK Board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect the micro and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
If the EVK board is used then the red led will blink.
MCX-N9XX-EVK
Hardware requirements
Mini/micro USB cable
MCX-N9XX-EVK Board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect the micro and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
If the EVK board is used then the red led will blink.
MCX-W72-EVK
Hardware requirements
Type-C USB cable
MCX-W72-EVK Board
Personal Computer
Board settings
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
And you will detect voltage toggle on J4.P31 of MB board. If the EVK board is used then the green led will blink.
MIMXRT700-EVK
Hardware requirements
Micro USB cable
MIMXRT700-EVK board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:: And you will find the LED BLUE is taking turns to shine.
GPIO Driver example
The LED is taking turns to shine
TWR-KM34Z50MV3
Hardware requirements
Mini USB cable
TWR-KM34Z50MV3 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
And you will find the 1 LED RED is taking turns to shine.
TWR-KM34Z75M
Hardware requirements
Mini USB cable
TWR-KM34Z75M board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the demo runs successfully, the following message is displayed in the terminal:
GPIO Driver example
The LED is blinking.
And you will find the LED RED is taking turns to shine.
TWR-KM35Z75M
Hardware requirements
Micro USB cable
TWR-KM35Z75M board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the demo runs successfully, the following message is displayed in the terminal:
GPIO Driver example
The LED is blinking.
And you will find the LED RED is taking turns to shine.
FRDM-MCXL255
Hardware requirements
Type-C USB cable
FRDM-MCXL255 board
Personal Computer
Board settings
Make sure you have solder bridges SJ1 and SJ2 set to
2-1 for the main core (cm33)
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port (J16) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
RED LED should be blinking.
The following lines are printed to the serial terminal when the demo program is executed.
GPIO Driver example
The LED is blinking.
FRDM-MCXA174
Hardware requirements
Type-C USB cable
FRDM-MCXA174 board
Personal Computer
Board settings
Prepare the Demo
Connect a USB Type-C cable between the host PC and MB board J22.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
And you will detect voltage toggle on the RED LED.
FRDM-MCXA344
Hardware requirements
Type-C USB cable
FRDM-MCXA344 board
Personal Computer
Board settings
Prepare the Demo
Connect a USB Type-C cable between the host PC and MB board J22.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
And you will detect voltage toggle on the RED LED.
KW47-LOC
Hardware requirements
Type-C USB cable
KW47-LOC Board
Personal Computer
Board settings
No special is needed.
Prepare the Demo
Connect a USB cable between the host PC and the LOC board J3.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
And you will detect voltage toggle on J2 Pin 1. If the LOC board is used then the blue led will blink.
MCXW72-LOC
Hardware requirements
Type-C USB cable
MCXW72-LOC Board
Personal Computer
Board settings
No special is needed.
Prepare the Demo
Connect a USB cable between the host PC and the LOC board J3.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
And you will detect voltage toggle on J2 Pin 1. If the LOC board is used then the blue led will blink.
FRDM-MCXA266
Hardware requirements
Type-C USB cable
FRDM-MCXA266 board
Personal Computer
Board settings
Prepare the Demo
Connect a USB Type-C cable between the host PC and MB board J22.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
And you will detect voltage toggle on the RED LED.
FRDM-MCXA366
Hardware requirements
Type-C USB cable
FRDM-MCXA366 board
Personal Computer
Board settings
Prepare the Demo
Connect a USB Type-C cable between the host PC and MB board J22.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
And you will detect voltage toggle on the RED LED.
FRDM-MCXW72
Hardware requirements
Type-C USB cable
FRDM-MCXW72 Board
Personal Computer
Board settings
No special is needed.
Prepare the Demo
Connect a USB cable between the host PC and the FRDM board J10.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
And you will detect voltage toggle on J1 Pin 6. If the FRDM board is used then the blue led will blink.
FRDM-MCXA577
Hardware requirements
Type-C USB cable
FRDM-MCXA577 board
Personal Computer
Board settings
Prepare the Demo
Connect a USB Type-C cable between the host PC and MB board J22.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
And you will detect voltage toggle on the RED LED.
FRDM-MCXC162
Hardware requirements
Type-C USB cable
FRDM-MCXC162 board
Personal Computer
Board settings
Prepare the Demo
Connect a USB Type-C cable between the host PC and MB board J22.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
And you will detect voltage toggle on the RED LED.
FRDM-KW43
Hardware requirements
Type-C USB cable
FRDM-KW43 Board
Personal Computer
Board settings
Prepare the Demo
Connect a USB cable between the host PC and the FRDM board J28.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
If the FRDM board is used then the red led will blink.
FRDM-MCXW70
Hardware requirements
Type-C USB cable
FRDM-MCXW70 Board
Personal Computer
Board settings
Prepare the Demo
Connect a USB cable between the host PC and the FRDM board J28.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
If the FRDM board is used then the red led will blink.
FRDM-MCXA287
Hardware requirements
Type-C USB cable
FRDM-MCXA287 board
Personal Computer
Board settings
Prepare the Demo
Connect a USB Type-C cable between the host PC and MB board J22.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
GPIO Driver example
The LED is blinking.
And you will detect voltage toggle on the RED LED.