MCUXpresso SDK Documentation

xrdc#

Overview#

The xrdc example shows how to control the memory and peripheral access policy using XRDC.

In this example, one peripheral and a memory region are set to unaccessible, then the hardfault occurs.

Running the demo#

The log below shows the output of the example in the terminal window. NOTE The access address might be different by platforms.

XRDC example start
Set the peripheral not accessible
Violent access at address: 0x40032000
The peripheral is accessible now
Set the memory not accessible
Violent access at address: 0x08000000
The memory is accessible now
XRDC example Success

Supported Boards#