host_msd_command#
Overview#
This Host MSD example supports the UFI and SCSI U-disk device.
The application prints the attached device information when the U-disk device is attached.
The application executes UFI commands to test the attached device.
System Requirement#
Hardware requirements#
Mini/micro USB cable
USB A to micro AB cable
Hardware (Tower module/base board, and so on) for a specific device
Personal Computer (PC)
Software requirements#
The project path is:
<MCUXpresso_SDK_Install>/boards//usb_examples/usb_host_msd_command/ / .
The
is Bare Metal or FreeRTOS OS.
Getting Started#
Hardware Settings#
Set the hardware jumpers (Tower system/base module) to default settings.
Prepare the example#
Download the program to the target board.
Power off the target board and power on again.
Connect devices to the board.
For detailed instructions, see the appropriate board User’s Guide.
Run the example#
Connect the board UART to the PC and open the COM port in a terminal tool.
Make sure to use a USB HUB or an adapter with OTG functionality firstly. Plug in the U-disk device to the board. The attached information prints out in the terminal.
The test information prints in the terminal, “success” prints when one command succeeds and “fail” prints when one command fails. The test completes when there is a command fail or all the tests are done.
The following figure is an example for attaching one U-disk device.
To test throughput, set the MSD_THROUGHPUT_TEST_ENABLE to (1) in te file host_msd_command.h. An additional 64 K RAM is required to test the throughput. The macro is only supported on the TWR-K65F180M Tower System module and IAR.
The following figure is a throughput test example for attaching one U-disk device.
Throughput test only supports the TWR-K65F180M Tower System module.
Supported Boards#
FRDM-K22F
Getting Started
Hardware Settings
The Jumper settings:\n J22 1-2.
LPCXpresso55S69
Getting Started
Hardware Settings
The Jumper settings:\n J6 1-2 and J7 open for high speed mode, J6 2-3 and J7 shunt for full speed mode.
The external +5V power only port shoud be connected with a power USB cable to provide USB VBUS.
LPCXpresso54S018
Getting Started
Hardware Settings
The Jumper settings:\n J9 1-2 high speed mode,2-3 full speed mode; J10 open high speed, shunt full speed; J11 2-3, J12 2-3, J13 2-3 , need provide external power through J1.
LPCXpresso55S16
Getting Started
Hardware Settings
The Jumper settings:\n JP20 1-2, JP21 1-2 and JP22 1-2 for chip power. JP2 1-2 and JS2 shunt for full speed mode, JP2 2-3 and JS2 open for high speed mode.
The external +5V power only port shoud be connected with a power USB cable to provide USB VBUS.
LPCXpresso54S018M
Getting Started
Hardware Settings
The Jumper settings:\n J9 1-2 high speed mode,2-3 full speed mode; J10 open high speed, shunt full speed; J11 2-3, J12 2-3, J13 2-3 , need provide external power through J1.
LPCXpresso55S28
Getting Started
Hardware Settings
The Jumper settings:\n J6 1-2 and J7 open for high speed mode, J6 2-3 and J7 shunt for full speed mode.
The external +5V power only port shoud be connected with a power USB cable to provide USB VBUS.
LPCXpresso54628
Getting Started
Hardware Settings
The Jumper settings:\n J9 1-2 high speed mode,2-3 full speed mode; J10 open high speed, shunt full speed; J11 2-3, J12 2-3, J13 2-3 , need provide external power through J1.
MCX-N5XX-EVK
Getting Started
Hardware Settings
The Jumper settings:\n J21 1-2.
FRDM-K32L2A4S
Getting Started
Hardware Settings
The Jumper settings:\n J9 1-2, J16 1-2.
MCX-N9XX-EVK
Getting Started
Hardware Settings
The Jumper settings:\n J21 1-2.