MCUXpresso SDK Documentation

se05x_cloud_azure

se05x_cloud_azure#

Overview#

This demo demonstrates connection to Azure IoTHub using pre-provisioned device credentials and demonstrates publish/subscribe procedure using MQTT.

Supported Boards#

LPCXpresso55S69
Hardware requirements
  • Mini/micro USB cable

  • LPCXpresso55s69 board

  • Personal Computer

  • CMWC1ZZABR-107-EVB by muRata

  • OM- SE050ARD or OM- SE051ARD

Board settings

Jumper settings for OM- SE050ARD & OM- SE051ARD: -J14 3-4 (Default): EdgeLock SE05x_VCC pin routed to SE05X_VOUT pin -J15 3-4 (Default): I2C target SDA connection -J17 3-4 (Default): I2C target SCL connection

Prerequisites
  • Active azure account with iot hub created

  • The Plug & Trust MW package can be downloaded from https://www.nxp.com/products/security-and-authentication/authentication/edgelock-se050-plug-and-trust-secure-element-family-enhanced-iot-security-with-high-flexibility:SE050#design-resources

  • Any Serial communicator

  • Flash VCOM binary on the device at flash address 0x00000000. VCOM binary se05x_vcom-T1oI2C-.bin can found in Plug & Trust MW package :simw-top\binaries\MCU folder.

Creating a device on azure IoT Hub portal
  1. Navigate to the Dashboard –> –> “Devices”

  2. Add a new device (e.g. device1), and for its authentication type choose X.509 CA Signed

Creating and updating device keys and certificates to SE
  1. Check the vcom port number

  2. Go to the EdgeLock SE05x Plug & Trust middleware ..\simw-top\binaries\PCWindows\ssscli folder and call:

    Provision_AZURE.exe note: is detected vcom port

  3. Certificates and Keys are generated at simw-top/binaries/PCWindows/ssscli/azure

Uploading root certificates to IoT Hub
  1. On Azure IoT Hub portal, Navigate to Dashboard --> <Your IoT Hub> --> Certificates. Click on Add

  2. Enter a friendly name and upload the root certificate created in the previous step. Location - simw-top\pycli\Provisioning\azure\RootCA.cer -> Save

  3. Your certificate will show in the Certificate Explorer list. Click on certificate added

  4. In Certificate Details, click Generate Verification Code

  5. The provisioning service creates a Verification Code that you can use to validate the certificate ownership. Copy the code to your clipboard

  6. Use the verification_certificate.py to generate a verify certificate (verifyCert4.cer) ::

     cd simw-top\pycli\Provisioning
     python verification_certificate.py <RootCA_Certificate> <RootCA_Keypair> <Verification Code>
    
  7. On Azure portal -> Certificate Details, upload the verifyCert4.cer file generated and click Verify. STATUS of your certificate should change to Verified in the Certificate Explorer list

Running the Demo
  1. Update AZURE_IOT_HUB_NAME and AZURE_DEVICE_NAME in <PROJECT>\source\azure_iot_config.h with your details.

  2. Update clientcredentialWIFI_SSID and clientcredentialWIFI_PASSWORD in <PROJECT>\se_hostlib\demos\ksdk\common\wifi_config.h with your wifi credentials.

  3. Connect your board to open network on wifi.

  4. Build the project and flash the binary on board.

The log below shows the output of the demo in the terminal window. The log can be different based on your local network configuration. App :INFO :PlugAndTrust_v04.04.00_20230811 sss :INFO :atr (Len=35) 01 A0 00 00 03 96 04 03 E8 00 FE 02 0B 03 E8 00 01 00 00 00 00 64 13 88 0A 00 65 53 45 30 35 31 00 00 00 sss :WARN :Communication channel is Plain. sss :WARN :!!!Not recommended for production use.!!! App :INFO :Azure Secure Element example …

App :INFO :Turning WIFI ON App :INFO :Connecting to network:iot_wifi_ssid App :INFO :Wi-Fi is connecting…

App :INFO :Wi-Fi is connecting…

App :INFO :Wi-Fi is connecting…

App :INFO :Wi-Fi is connecting…

App :INFO :Wi-Fi is connected to: iot_wifi_ssid, IP Address: 192.168.0.106

[INFO] Create a TCP connection to NXPPNT.azure-devices.net:8883. [INFO] (Network connection 0x20009288) TLS handshake successful. [INFO] (Network connection 0x20009288) Connection to NXPPNT.azure-devices.net established. [INFO] MQTT connection established with the broker. [INFO] MQTT connection successfully established with broker.

[INFO] A clean MQTT connection is established. Cleaning up all the stored outgoing publishes.

App :INFO :MQTT Connection successfully established [INFO] Attempt to subscribe to the MQTT topic devices/377819357023377568295309/messages/devicebound[DEBUG] Encoded size for length 60 is 1 bytes.

App :INFO :MQTT Subscribed [INFO] the published payload:{“msg” : “hello from SDK QOS0 : 0”} [INFO] PUBLISH sent for topic devices/377819357023377568295309/messages/events/ to broker with packApp :INFO :Published message {“msg” : “hello from SDK QOS0 : 0”} App :INFO :AZURE demo passed App :INFO :Demo Example Finished