capt_basic_continuous#
Overview#
This example shows how to capture touch data using CAPT continuous mode. CAP polls and samples the touch pad data round by round, in each round, all the enabled pins are sampled one by one. To monitor one pad sample finished, both the yes_touch and no_touch interrupt is enabled. The poll done interrupt is enabled to monitor the poll round finished. The delay period between two polling round is configurable, in this example, the delay period is set to about 0.5s. When the example runs, the sampled data is shown in the terminal, and update every about 0.5s. When electrode plate is touched, the sampled data changes too.