MCUXpresso SDK Documentation

rtc_example

rtc_example#

Overview#

The RTC project is a simple demonstration program of the SDK RTC driver. It sets up the RTC hardware block to trigger an alarm after a user specified time period. The test will set the current date and time to a predefined value. The alarm will be set with reference to this predefined date and time.

Supported Boards#

EVK-MIMXRT595
Hardware requirements
  • Micro USB cable

  • EVK-MIMXRT595 board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the RTC driver demo in the terminal window:

RTC example: set up time to wake up an alarm
Current datetime: 2014-12-25 19: 0: 0
Please input the number of second to wait for alarm
The second must be positive value
Alarm will occur at: 2014-12-25 19: 0: 5
EVK-MIMXRT685
Hardware requirements
  • Micro USB cable

  • EVK-MIMXRT685 board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the RTC driver demo in the terminal window:

RTC example: set up time to wake up an alarm
Current datetime: 2014-12-25 19: 0: 0
Please input the number of second to wait for alarm
The second must be positive value
Alarm will occur at: 2014-12-25 19: 0: 5
FRDM-MCXW23
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXW23 Board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the FRDM board J10.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the RTC driver demo in the terminal window:

RTC example: set up time to wake up an alarm
Current datetime: 2014-12-25 19: 0: 0
Please input the number of second to wait for alarm
The second must be positive value
Alarm will occur at: 2014-12-25 19: 0: 5
FRDM-RW612
Hardware requirements
  • Micro USB cable

  • FRDM-RW612 board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J10) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the RTC driver demo in the terminal window:

RTC example: set up time to wake up an alarm
Current datetime: 2014-12-25 19: 0: 0
Please input the number of second to wait for alarm
The second must be positive value
Alarm will occur at: 2014-12-25 19: 0: 5
LPCXpresso51U68
Hardware requirements
  • Mini/micro USB cable

  • LPCXpresso51U68 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J6) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the RTC driver demo in the terminal window:

RTC example: set up time to wake up an alarm
Current datetime: 2014-12-25 19: 0: 0
Please input the number of second to wait for alarm
The second must be positive value
Alarm will occur at: 2014-12-25 19: 0: 5
LPCXpresso54628
Hardware requirements
  • Micro USB cable

  • LPCXpresso54628 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the RTC driver demo in the terminal window:

RTC example: set up time to wake up an alarm
Current datetime: 2014-12-25 19: 0: 0
Please input the number of second to wait for alarm
The second must be positive value
Alarm will occur at: 2014-12-25 19: 0: 5
LPCXpresso54S018
Hardware requirements
  • Micro USB cable

  • LPCXpresso54S018 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

This demo is an external flash plain load demo, ROM will copy image in external flash to SRAMX to run:

  1. Build the demo to generate a bin file. Note: If need to generate bin file using MCUXpresso IDE, below steps need to be followed: Set in example Properties->C/C++ Build->Settings->Build steps->Post-build steps->Edit enbable arm-none-eabi-objcopy -v -O binary “&{BuildArtifactFileName}” “&{BuildArtifactFileBaseName}.bin”

      This plainload example linked the vector table to 0x00000000, but program to external flash 0x10000000.
    
  2. Program the bin file to external on board flash via SEGGER J-FLASH Lite(V6.22 or higher):

    a. Open SEGGER J-FLASH Lite, select device LPC54S018.

    b. Click the ‘Erase Chip’ to erase the extrenal flash.(if can not success, press SW4 button and reset the board, and try to erase again)

    c. Select the bin data file, set the ‘.bin/Erase Start’ address to 0x10000000, then click ‘Program Device’ Note: Please use above way to program the binary file built by armgcc tool chain to external flash. For IAR, KEIL, MCUXpresso IDE, you can use the IDE tool to program the external flash.
    The log below shows example output of the RTC driver demo in the terminal window:

RTC example: set up time to wake up an alarm
Current datetime: 2014-12-25 19: 0: 0
Please input the number of second to wait for alarm
The second must be positive value
Alarm will occur at: 2014-12-25 19: 0: 5
LPCXpresso54S018M
Hardware requirements
  • Micro USB cable

  • LPCXpresso54S018M board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

This demo is an external flash plain load demo, ROM will copy image in external flash to SRAMX to run:

  1. Build the demo to generate a bin file. Note: If need to generate bin file using MCUXpresso IDE, below steps need to be followed: Set in example Properties->C/C++ Build->Settings->Build steps->Post-build steps->Edit enbable arm-none-eabi-objcopy -v -O binary “&{BuildArtifactFileName}” “&{BuildArtifactFileBaseName}.bin”

      This plainload example linked the vector table to 0x00000000, but program to external flash 0x10000000.
    
  2. Program the bin file to external on board flash via SEGGER J-FLASH Lite(V6.22 or higher):

    a. Open SEGGER J-FLASH Lite, select device LPC54S018M.

    b. Click the ‘Erase Chip’ to erase the extrenal flash.(if can not success, press SW4 button and reset the board, and try to erase again)

    c. Select the bin data file, set the ‘.bin/Erase Start’ address to 0x10000000, then click ‘Program Device’ Note: Please use above way to program the binary file built by armgcc tool chain to external flash. For IAR, KEIL, MCUXpresso IDE, you can use the IDE tool to program the external flash.
    The log below shows example output of the RTC driver demo in the terminal window:

RTC example: set up time to wake up an alarm
Current datetime: 2014-12-25 19: 0: 0
Please input the number of second to wait for alarm
The second must be positive value
Alarm will occur at: 2014-12-25 19: 0: 5
LPCXpresso55S06
Hardware requirements
  • Micro USB cable

  • LPCXpresso55S06 board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a micro USB cable between the host PC and the LPC-Link USB port (J1) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the RTC driver demo in the terminal window:

RTC example: set up time to wake up an alarm
Current datetime: 2014-12-25 19: 0: 0
Please input the number of second to wait for alarm
The second must be positive value
Alarm will occur at: 2014-12-25 19: 0: 5
LPCXpresso55S16
Hardware requirements
  • Micro USB cable

  • LPCXpresso55S16 board

  • Personal Computer

Board settings

The jumper setting: Default jumpers configuration does not work, you will need to add JP20 and JP21 (JP22 optional for ADC use)

Prepare the Demo
  1. Connect a micro USB cable between the host PC and the LPC-Link USB port (J1) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the RTC driver demo in the terminal window:

RTC example: set up time to wake up an alarm
Current datetime: 2014-12-25 19: 0: 0
Please input the number of second to wait for alarm
The second must be positive value
Alarm will occur at: 2014-12-25 19: 0: 5
LPCXpresso55S28
Hardware requirements
  • Micro USB cable

  • LPCXpresso55S28 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

Note: MCUXpresso IDE project default debug console is semihost

  1. Connect a micro USB cable between the host PC and the LPC-Link USB port (P6) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the RTC driver demo in the terminal window:

RTC example: set up time to wake up an alarm
Current datetime: 2014-12-25 19: 0: 0
Please input the number of second to wait for alarm
The second must be positive value
Alarm will occur at: 2014-12-25 19: 0: 5
LPCXpresso55S69
Hardware requirements
  • Micro USB cable

  • LPCXpresso55s69 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

Note: MCUXpresso IDE project default debug console is semihost

  1. Connect a micro USB cable between the host PC and the LPC-Link USB port (P6) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the RTC driver demo in the terminal window:

RTC example: set up time to wake up an alarm
Current datetime: 2014-12-25 19: 0: 0
Please input the number of second to wait for alarm
The second must be positive value
Alarm will occur at: 2014-12-25 19: 0: 5
MIMXRT685-AUD-EVK
Hardware requirements
  • Micro USB cable

  • MIMXRT685-AUD-EVK board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the RTC driver demo in the terminal window:

RTC example: set up time to wake up an alarm
Current datetime: 2014-12-25 19: 0: 0
Please input the number of second to wait for alarm
The second must be positive value
Alarm will occur at: 2014-12-25 19: 0: 5
RD-RW612-BGA
Hardware requirements
  • Micro USB cable

  • RD-RW612-BGA board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J7) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the RTC driver demo in the terminal window:

RTC example: set up time to wake up an alarm
Current datetime: 2014-12-25 19: 0: 0
Please input the number of second to wait for alarm
The second must be positive value
Alarm will occur at: 2014-12-25 19: 0: 5
MCXW23-EVK
Hardware requirements
  • Mini/micro USB cable

  • MCXW23-EVK Board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board J33.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the RTC driver demo in the terminal window:

RTC example: set up time to wake up an alarm
Current datetime: 2014-12-25 19: 0: 0
Please input the number of second to wait for alarm
The second must be positive value
Alarm will occur at: 2014-12-25 19: 0: 5