multi_peripherals_test#
Overview#
The multi-peripherals-test demo application does the basic peripheral test on board. This demo will test audio, usb, led, button, sdcard, accelerometer and rtc. To test audio function, connect an audio source, for example from a mobile phone or PC, to Line-IN connector, connect a headphone or speaker to Line-Out connector. Then the input audio can be heared in the headphone or speaker. To test usb, connect a USB cable between the PC and board’s high speed connector, the cursor on the PC will move in a square pattern. To test sdcard function, insert a uSD memory card in to the connector, then the test result will be printed, please make sure the message is not a failed message. Please verify the green LED in the RGB-LED flashed with a 1Hz rate. This indicates that the RTC crystal works.
Supported Boards#
LPCXpresso55S16
Hardware requirements
Micro USB cable
LPCXpresso55S16 board
Personal Computer
headphones with 3.5 mm stereo jack
source of sound (line output to 3.5 mm stereo jack)
Board settings
No special is needed.
Prepare the Demo
Note: MCUXpresso IDE project default debug console is semihost
Connect headphones to Audio HP / Line-Out connector.
Connect source of sound(from PC or Smart phone) to Audio Line-In connector.
Connect a micro USB cable between the PC host and the LPC-Link USB port (J8) on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
Multi-peripheral Test!
AUDIO Loopback started!
Headphones will play what is input into Audio Line-In connector.
Accelerometer: Found Accelerometer!
USB device HID mouse test
Plug-in the device, which is running mouse test, into the PC.A HID-compliant mouse is enumerated in the Device Manager.
The mouse arrow is moving on PC screen in the rectangular rotation.
Press the WAKEUP button, the red LED will flash. Press the ISP button, the blue LED will flash. Press the USER button, the green LED will constant on.
LPCXpresso55S28
Hardware requirements
Micro USB cable
LPCXpresso55S28 board
Personal Computer
SD card
headphones with 3.5 mm stereo jack
source of sound (line output to 3.5 mm stereo jack)
Board settings
Insert the card(FAT32 formatted with testfile.txt in the root) into the card slot.
Prepare the Demo
Note: MCUXpresso IDE project default debug console is semihost
Connect headphones to Audio HP / Line-Out connector.
Connect source of sound(from PC or Smart phone) to Audio Line-In connector.
Connect a micro USB cable between the PC host and the LPC-Link USB port (J8) on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Insert sdcard into sdcard.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
Multi-peripheral Test!
Start datetime: 2020- 9-24 19:15: 0
AUDIO Loopback started!
Headphones will play what is input into Audio Line-In connector.
Accelerometer: Found Accelerometer!
USB device HID mouse test
Plug-in the device, which is running mouse test, into the PC.A HID-compliant mouse is enumerated in the Device Manager.
The mouse arrow is moving on PC screen in the rectangular rotation.
SDCARD: Write/read file ......
Write to testfile.txt.
Read from testfile.txt.
Compare the read/write content......
SDCARD Tested OK!
Press the WAKEUP button, the red LED will flash. Press the ISP button, the blue LED will flash. Press the USER button, the green LED will constant on.
LPCXpresso55S69
Hardware requirements
Micro USB cable
LPCXpresso55S69 board
Personal Computer
SD card
headphones with 3.5 mm stereo jack
source of sound (line output to 3.5 mm stereo jack)
Board settings
Insert the card(FAT32 formatted with testfile.txt in the root) into the card slot.
Prepare the Demo
Note: MCUXpresso IDE project default debug console is semihost
Connect headphones to Audio HP / Line-Out connector.
Connect source of sound(from PC or Smart phone) to Audio Line-In connector.
Connect a micro USB cable between the PC host and the LPC-Link USB port (J8) on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Insert sdcard into sdcard.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
Multi-peripheral Test!
Start datetime: 2020- 9-24 19:15: 0
AUDIO Loopback started!
Headphones will play what is input into Audio Line-In connector.
Accelerometer: Found Accelerometer!
USB device HID mouse test
Plug-in the device, which is running mouse test, into the PC.A HID-compliant mouse is enumerated in the Device Manager.
The mouse arrow is moving on PC screen in the rectangular rotation.
SDCARD: Write/read file ......
Write to testfile.txt.
Read from testfile.txt.
Compare the read/write content......
SDCARD Tested OK!
Press the WAKEUP button, the red LED will flash. Press the ISP button, the blue LED will flash. Press the USER button, the green LED will constant on.