MCUXpresso SDK Documentation

lpadc_light_sensor

lpadc_light_sensor#

Overview#

The lpadc_light_sensor example shows how to use the LPADC driver to measure the voltage value in the circuit with a light sensor. In this example, the specific ADC channel has been connected into the circuit by board design. When running the project, typing any key into the debug console would trigger the conversion. The execution would check the FIFO valid flag in a loop until the flag is asserted, which means the conversion is completed. Then read the conversion result value and print it to the debug console.

Supported Boards#

FRDM-MCXW71
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXW71 Board

  • Personal Computer

Board settings

This example project uses LPADC0 channel 6 to collect the output voltage of the circuit, which has a light sensor, and the output voltage is proportional to the light illuminance. When the illuminance increases, the output voltage increases, and the value printed by the terminal is also larger.

Prepare the Demo
  1. Connect a USB cable between the host PC and the FRDM board J10.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The following lines are printed to the serial terminal when the demo program is executed.

LPADC Light Sensor Example.
LPADC Reference Voltage Config Done!
LPADC Config Done, Full Range: 65536
Please press any key to get the light sensor value.
light sensor value: xxxx
FRDM-MCXW72
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXW72 Board

  • Personal Computer

Board settings

This example project uses LPADC0 channel 6 to collect the output voltage of the circuit, which has a light sensor, and the output voltage is proportional to the light illuminance. When the illuminance increases, the output voltage increases, and the value printed by the terminal is also larger.

Prepare the Demo
  1. Connect a USB cable between the host PC and the FRDM board J10.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The following lines are printed to the serial terminal when the demo program is executed.

LPADC Light Sensor Example.
LPADC Config Done, Full Range: 65536
Please press any key to get the light sensor value.
light sensor value: xxxx
MCX-N5XX-EVK
Hardware requirements
  • Micro USB cable

  • MCX-N5XX-EVK Board

  • Personal Computer

Board settings

This example project uses LPADC1 channel 0 to collect the output voltage of the circuit, which has a light sensor, and the output voltage is proportional to the light illuminance. When the illuminance increases, the output voltage increases, and the value printed by the terminal is also larger.

Note that on some MCX-N5XX-EVK boards, the circuit that has a light sensor does not weld up the resistor SH1 and capacitor C202; before running this example, please check it.

Prepare the Demo
  1. Connect the micro USB cable between the PC host and the USB ports on the board.

  2. Open a serial terminal on PC for the serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The following lines are printed to the serial terminal when the demo program is executed.

LPADC Light Sensor Example.
LPADC Reference Voltage Config Done!
LPADC Config Done, Full Range: 65536
Please press any key to get the light sensor value.
light sensor value: xxxx
MCX-N9XX-EVK
Hardware requirements
  • Micro USB cable

  • MCX-N9XX-EVK Board

  • Personal Computer

Board settings

This example project uses LPADC1 channel 0 to collect the output voltage of the circuit, which has a light sensor, and the output voltage is proportional to the light illuminance. When the illuminance increases, the output voltage increases, and the value printed by the terminal is also larger.

Note that on some MCX-N9XX-EVK boards, the circuit that has a light sensor does not weld up the resistor SH1 and capacitor C202; before running this example, please check it.

Prepare the Demo
  1. Connect the micro USB cable between the PC host and the USB ports on the board.

  2. Open a serial terminal on PC for the serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The following lines are printed to the serial terminal when the demo program is executed.

LPADC Light Sensor Example.
LPADC Reference Voltage Config Done!
LPADC Config Done, Full Range: 65536
Please press any key to get the light sensor value.
light sensor value: xxxx