crc#
Overview#
The CRC Example project is a demonstration program that generates checksums for an ASCII string. Several CRC protocols are implemented using the CRC driver API.
Running the demo#
Example output on terminal:
Test same string base on different CRC protocols.
Test string: 123456789 1.CRC-16 : 0x2189 2.CRC-32 : 0x340BC6