mcg_fee_blpe#
Overview#
The fee_bple example shows how to use MCG driver to change from FEE mode to BLPE mode:
How to use the mode functions for MCG mode switch.
How to use the frequency functions to get current MCG frequency.
Work flow Boot to Fee mode from default reset mode Change from FEE -> FBE -> BLPE Change back BLPE -> FBE -> FEE Get System clock in FEE mode to blink LED
In this example, because the debug console’s clock frequency may change, so the example running information is not output from debug console. Here the LED blinks to show that the example finished successfully.
Supported Boards#
FRDM-K22F
Hardware requirements
Mini/Micro USB cable
FRDMK22F board
Personal Computer
Board settings
No special board settings.
Prepare the Demo
Connect a mini/micro USB cable between the PC host and the OpenSDA USB port on FRDMK22F board.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. For detailed instructions, see Getting Started with Software Development Kit for K22F.
Running the demo
When the demo runs successfully, the board’s LED will blink.
TWR-KM34Z50MV3
Hardware requirements
Mini USB cable
TWR-KM34Z50MV3 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the demo runs successfully, the board’s LED will blink.
TWR-KM34Z75M
Hardware requirements
Mini USB cable
TWR-KM34Z75M board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the demo runs successfully, the board’s LED will blink.
TWR-KM35Z75M
Hardware requirements
Micro USB cable
TWR-KM35Z75M board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the demo runs successfully, the board’s LED will blink.