MCUXpresso SDK Documentation

els_pkc_fips_st

els_pkc_fips_st#

Overview#

This application is executing tests using els_pkc crypto library on RW61x board w.r.t. the NIST Cryptographic Algorithm Validation Program (CAVP). The user is able to specfiy, which algorithms should get tested - by default all algorithms are tested. The test vectors are specified as global variables in the respective files.

Supported Boards#

RD-RW612-BGA
Hardware requirements
  • Micro USB cable

  • RD-RW612-BGA board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J7) on the board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the example.

Running the demo

When the demo runs successfully, the terminal will display similar information like the following:

START OF ELS PKC FIPS SELF-TEST… HW ACCELERATION ALGORITHM INFORMATION: ECB DRBG: ELS CTR DRBG: ELS CKDF SP800-108: ELS HKDF RFC5869: ELS ECDSA NISTP 256: ELS ECDSA NISTP 384: PKC ECDSA NISTP 521: PKC EDDSA ED25519: PKC ECDH NISTP 256: ELS ECDH NISTP 384: PKC ECDH NISTP 521: PKC ECC KEYGEN NISTP 256: ELS ECC KEYGEN NISTP 384: PKC ECC KEYGEN NISTP 521: PKC RSA-PKCS15-2048: PKC RSA-PKCS15-3072: PKC RSA-PKCS15-4096: PKC RSA-PSS-2048: PKC RSA-PSS-3072: PKC RSA-PSS-4096: PKC AES-CCM-128: ELS AES-CCM-256: ELS AES-GCM-128: ELS AES-GCM-192: ELS AES-GCM-256: ELS AES-CTR-128: ELS AES-CTR-192: ELS AES-CTR-256: ELS AES-ECB-128: ELS AES-ECB-192: ELS AES-ECB-256: ELS AES-CBC-128: ELS AES-CBC-192: ELS AES-CBC-256: ELS AES-CMAC-128: ELS AES-CMAC-256: ELS HMAC-SHA224: SOFTWARE IMPLEMENTATION HMAC-SHA256: ELS HMAC-SHA384: SOFTWARE IMPLEMENTATION HMAC-SHA512: SOFTWARE IMPLEMENTATION SHA224: ELS SHA256: ELS SHA384: ELS SHA512: ELS

EXECUTING ECB-DRBG SELF-TEST

  • ECB-DRBG KAT SUCCESS EXECUTING CTR-DRBG SELF-TEST

  • CTR-DRBG KAT SUCCESS EXECUTING CKDF-SP800-108 SELF-TEST

  • CKDF-SP800-108 KAT SUCCESS EXECUTING HKDF-SP800-56C SELF-TEST

  • HKDF-SP800-56C KAT SUCCESS EXECUTING HKDF-RFC5869 SELF-TEST

  • HKDF-RFC5869 KAT SUCCESS EXECUTING NON-DET ECDSA-256P SELF-TEST

  • NON-DET ECDSA-256P PCT SUCCESS EXECUTING ECDSA-384P SELF-TEST

  • ECDSA-384P SIGN KAT SUCCESS

  • ECDSA-384P VERIFY KAT SUCCESS EXECUTING ECDSA-521P SELF-TEST

  • ECDSA-521P SIGN KAT SUCCESS

  • ECDSA-521P VERIFY KAT SUCCESS EXECUTING ED25519 SELF-TEST

  • ED25519 SIGN KAT SUCCESS

  • ED25519 VERIFY KAT SUCCESS EXECUTING ECDH-256P SELF-TEST

  • ECDH-256P KAT SUCCESS EXECUTING ECDH-384P SELF-TEST

  • ECDH-384P KAT SUCCESS EXECUTING ECDH-521P SELF-TEST

  • ECDH-521P KAT SUCCESS EXECUTING ECC-KEYGEN-256P SELF-TEST

  • ECC-KEYGEN-256P PCT SUCCESS EXECUTING ECC-KEYGEN-384P SELF-TEST

  • ECC-KEYGEN-384P PCT SUCCESS EXECUTING ECC-KEYGEN-521P SELF-TEST

  • ECC-KEYGEN-521P PCT SUCCESS EXECUTING RSA-PKCS15-2048 SELF-TEST

  • RSA-PKCS15-2048 SIGN KAT SUCCESS

  • RSA-PKCS15-2048 VERIFY KAT SUCCESS EXECUTING RSA-PKCS15-3072 SELF-TEST

  • RSA-PKCS15-3072 SIGN KAT SUCCESS

  • RSA-PKCS15-3072 VERIFY KAT SUCCESS EXECUTING RSA-PKCS15-4096 SELF-TEST

  • RSA-PKCS15-4096 SIGN KAT SUCCESS

  • RSA-PKCS15-4096 VERIFY KAT SUCCESS EXECUTING RSA-PSS-2048 SELF-TEST

  • RSA-PSS-2048 SIGN KAT SUCCESS

  • RSA-PSS-2048 VERIFY KAT SUCCESS EXECUTING RSA-PSS-3072 SELF-TEST

  • RSA-PSS-3072 SIGN KAT SUCCESS

  • RSA-PSS-3072 VERIFY KAT SUCCESS EXECUTING RSA-PSS-4096 SELF-TEST

  • RSA-PSS-4096 SIGN KAT SUCCESS

  • RSA-PSS-4096 VERIFY KAT SUCCESS EXECUTING AES-CCM-128 SELF-TEST

  • AES-CCM-128 ENCRYPT KAT SUCCESS

  • AES-CCM-128 DECRYPT KAT SUCCESS EXECUTING AES-CCM-256 SELF-TEST

  • AES-CCM-256 ENCRYPT KAT SUCCESS

  • AES-CCM-256 DECRYPT KAT SUCCESS EXECUTING AES-GCM-128 SELF-TEST

  • AES-GCM-128 ENCRYPT KAT SUCCESS

  • AES-GCM-128 DECRYPT KAT SUCCESS EXECUTING AES-GCM-192 SELF-TEST

  • AES-GCM-192 ENCRYPT KAT SUCCESS

  • AES-GCM-192 DECRYPT KAT SUCCESS EXECUTING AES-GCM-256 SELF-TEST

  • AES-GCM-256 ENCRYPT KAT SUCCESS

  • AES-GCM-256 DECRYPT KAT SUCCESS EXECUTING AES-CTR-128 SELF-TEST

  • AES-CTR-128 ENCRYPT KAT SUCCESS

  • AES-CTR-128 DECRYPT KAT SUCCESS EXECUTING AES-CTR-192 SELF-TEST

  • AES-CTR-192 ENCRYPT KAT SUCCESS

  • AES-CTR-192 DECRYPT KAT SUCCESS EXECUTING AES-CTR-256 SELF-TEST

  • AES-CTR-256 ENCRYPT KAT SUCCESS

  • AES-CTR-256 DECRYPT KAT SUCCESS EXECUTING AES-ECB-128 SELF-TEST

  • AES-ECB-128 ENCRYPT KAT SUCCESS

  • AES-ECB-128 DECRYPT KAT SUCCESS EXECUTING AES-ECB-192 SELF-TEST

  • AES-ECB-192 ENCRYPT KAT SUCCESS

  • AES-ECB-192 DECRYPT KAT SUCCESS EXECUTING AES-ECB-256 SELF-TEST

  • AES-ECB-256 ENCRYPT KAT SUCCESS

  • AES-ECB-256 DECRYPT KAT SUCCESS EXECUTING AES-CBC-128 SELF-TEST

  • AES-CBC-128 ENCRYPT KAT SUCCESS

  • AES-CBC-128 DECRYPT KAT SUCCESS EXECUTING AES-CBC-192 SELF-TEST

  • AES-CBC-192 ENCRYPT KAT SUCCESS

  • AES-CBC-192 DECRYPT KAT SUCCESS EXECUTING AES-CBC-256 SELF-TEST

  • AES-CBC-256 ENCRYPT KAT SUCCESS

  • AES-CBC-256 DECRYPT KAT SUCCESS EXECUTING AES-CMAC-128 SELF-TEST

  • AES-CMAC-128 KAT SUCCESS EXECUTING AES-CMAC-256 SELF-TEST

  • AES-CMAC-256 KAT SUCCESS EXECUTING HMAC-SHA224 SELF-TEST

  • HMAC-SHA224 KAT SUCCESS EXECUTING HMAC-SHA256 SELF-TEST

  • HMAC-SHA256 KAT SUCCESS EXECUTING HMAC-SHA384 SELF-TEST

  • HMAC-SHA384 KAT SUCCESS EXECUTING HMAC-SHA512 SELF-TEST

  • HMAC-SHA512 KAT SUCCESS EXECUTING SHA224 SELF-TEST

  • SHA224 KAT SUCCESS EXECUTING SHA256 SELF-TEST

  • SHA256 KAT SUCCESS EXECUTING SHA384 SELF-TEST

  • SHA384 KAT SUCCESS EXECUTING SHA512 SELF-TEST

  • SHA512 KAT SUCCESS

END OF ELS PKC FIPS SELF-TEST

FRDM-RW612
Hardware requirements
  • Micro USB cable

  • FRDM-RW612 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J10) on the board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the example.

Running the demo

When the demo runs successfully, the terminal will display similar information like the following:

START OF ELS PKC FIPS SELF-TEST… HW ACCELERATION ALGORITHM INFORMATION: ECB DRBG: ELS CTR DRBG: ELS CKDF SP800-108: ELS HKDF RFC5869: ELS ECDSA NISTP 256: ELS ECDSA NISTP 384: PKC ECDSA NISTP 521: PKC EDDSA ED25519: PKC ECDH NISTP 256: ELS ECDH NISTP 384: PKC ECDH NISTP 521: PKC ECC KEYGEN NISTP 256: ELS ECC KEYGEN NISTP 384: PKC ECC KEYGEN NISTP 521: PKC RSA-PKCS15-2048: PKC RSA-PKCS15-3072: PKC RSA-PKCS15-4096: PKC RSA-PSS-2048: PKC RSA-PSS-3072: PKC RSA-PSS-4096: PKC AES-CCM-128: ELS AES-CCM-256: ELS AES-GCM-128: ELS AES-GCM-192: ELS AES-GCM-256: ELS AES-CTR-128: ELS AES-CTR-192: ELS AES-CTR-256: ELS AES-ECB-128: ELS AES-ECB-192: ELS AES-ECB-256: ELS AES-CBC-128: ELS AES-CBC-192: ELS AES-CBC-256: ELS AES-CMAC-128: ELS AES-CMAC-256: ELS HMAC-SHA224: SOFTWARE IMPLEMENTATION HMAC-SHA256: ELS HMAC-SHA384: SOFTWARE IMPLEMENTATION HMAC-SHA512: SOFTWARE IMPLEMENTATION SHA224: ELS SHA256: ELS SHA384: ELS SHA512: ELS

EXECUTING ECB-DRBG SELF-TEST

  • ECB-DRBG KAT SUCCESS EXECUTING CTR-DRBG SELF-TEST

  • CTR-DRBG KAT SUCCESS EXECUTING CKDF-SP800-108 SELF-TEST

  • CKDF-SP800-108 KAT SUCCESS EXECUTING HKDF-SP800-56C SELF-TEST

  • HKDF-SP800-56C KAT SUCCESS EXECUTING HKDF-RFC5869 SELF-TEST

  • HKDF-RFC5869 KAT SUCCESS EXECUTING NON-DET ECDSA-256P SELF-TEST

  • NON-DET ECDSA-256P PCT SUCCESS EXECUTING ECDSA-384P SELF-TEST

  • ECDSA-384P SIGN KAT SUCCESS

  • ECDSA-384P VERIFY KAT SUCCESS EXECUTING ECDSA-521P SELF-TEST

  • ECDSA-521P SIGN KAT SUCCESS

  • ECDSA-521P VERIFY KAT SUCCESS EXECUTING ED25519 SELF-TEST

  • ED25519 SIGN KAT SUCCESS

  • ED25519 VERIFY KAT SUCCESS EXECUTING ECDH-256P SELF-TEST

  • ECDH-256P KAT SUCCESS EXECUTING ECDH-384P SELF-TEST

  • ECDH-384P KAT SUCCESS EXECUTING ECDH-521P SELF-TEST

  • ECDH-521P KAT SUCCESS EXECUTING ECC-KEYGEN-256P SELF-TEST

  • ECC-KEYGEN-256P PCT SUCCESS EXECUTING ECC-KEYGEN-384P SELF-TEST

  • ECC-KEYGEN-384P PCT SUCCESS EXECUTING ECC-KEYGEN-521P SELF-TEST

  • ECC-KEYGEN-521P PCT SUCCESS EXECUTING RSA-PKCS15-2048 SELF-TEST

  • RSA-PKCS15-2048 SIGN KAT SUCCESS

  • RSA-PKCS15-2048 VERIFY KAT SUCCESS EXECUTING RSA-PKCS15-3072 SELF-TEST

  • RSA-PKCS15-3072 SIGN KAT SUCCESS

  • RSA-PKCS15-3072 VERIFY KAT SUCCESS EXECUTING RSA-PKCS15-4096 SELF-TEST

  • RSA-PKCS15-4096 SIGN KAT SUCCESS

  • RSA-PKCS15-4096 VERIFY KAT SUCCESS EXECUTING RSA-PSS-2048 SELF-TEST

  • RSA-PSS-2048 SIGN KAT SUCCESS

  • RSA-PSS-2048 VERIFY KAT SUCCESS EXECUTING RSA-PSS-3072 SELF-TEST

  • RSA-PSS-3072 SIGN KAT SUCCESS

  • RSA-PSS-3072 VERIFY KAT SUCCESS EXECUTING RSA-PSS-4096 SELF-TEST

  • RSA-PSS-4096 SIGN KAT SUCCESS

  • RSA-PSS-4096 VERIFY KAT SUCCESS EXECUTING AES-CCM-128 SELF-TEST

  • AES-CCM-128 ENCRYPT KAT SUCCESS

  • AES-CCM-128 DECRYPT KAT SUCCESS EXECUTING AES-CCM-256 SELF-TEST

  • AES-CCM-256 ENCRYPT KAT SUCCESS

  • AES-CCM-256 DECRYPT KAT SUCCESS EXECUTING AES-GCM-128 SELF-TEST

  • AES-GCM-128 ENCRYPT KAT SUCCESS

  • AES-GCM-128 DECRYPT KAT SUCCESS EXECUTING AES-GCM-192 SELF-TEST

  • AES-GCM-192 ENCRYPT KAT SUCCESS

  • AES-GCM-192 DECRYPT KAT SUCCESS EXECUTING AES-GCM-256 SELF-TEST

  • AES-GCM-256 ENCRYPT KAT SUCCESS

  • AES-GCM-256 DECRYPT KAT SUCCESS EXECUTING AES-CTR-128 SELF-TEST

  • AES-CTR-128 ENCRYPT KAT SUCCESS

  • AES-CTR-128 DECRYPT KAT SUCCESS EXECUTING AES-CTR-192 SELF-TEST

  • AES-CTR-192 ENCRYPT KAT SUCCESS

  • AES-CTR-192 DECRYPT KAT SUCCESS EXECUTING AES-CTR-256 SELF-TEST

  • AES-CTR-256 ENCRYPT KAT SUCCESS

  • AES-CTR-256 DECRYPT KAT SUCCESS EXECUTING AES-ECB-128 SELF-TEST

  • AES-ECB-128 ENCRYPT KAT SUCCESS

  • AES-ECB-128 DECRYPT KAT SUCCESS EXECUTING AES-ECB-192 SELF-TEST

  • AES-ECB-192 ENCRYPT KAT SUCCESS

  • AES-ECB-192 DECRYPT KAT SUCCESS EXECUTING AES-ECB-256 SELF-TEST

  • AES-ECB-256 ENCRYPT KAT SUCCESS

  • AES-ECB-256 DECRYPT KAT SUCCESS EXECUTING AES-CBC-128 SELF-TEST

  • AES-CBC-128 ENCRYPT KAT SUCCESS

  • AES-CBC-128 DECRYPT KAT SUCCESS EXECUTING AES-CBC-192 SELF-TEST

  • AES-CBC-192 ENCRYPT KAT SUCCESS

  • AES-CBC-192 DECRYPT KAT SUCCESS EXECUTING AES-CBC-256 SELF-TEST

  • AES-CBC-256 ENCRYPT KAT SUCCESS

  • AES-CBC-256 DECRYPT KAT SUCCESS EXECUTING AES-CMAC-128 SELF-TEST

  • AES-CMAC-128 KAT SUCCESS EXECUTING AES-CMAC-256 SELF-TEST

  • AES-CMAC-256 KAT SUCCESS EXECUTING HMAC-SHA224 SELF-TEST

  • HMAC-SHA224 KAT SUCCESS EXECUTING HMAC-SHA256 SELF-TEST

  • HMAC-SHA256 KAT SUCCESS EXECUTING HMAC-SHA384 SELF-TEST

  • HMAC-SHA384 KAT SUCCESS EXECUTING HMAC-SHA512 SELF-TEST

  • HMAC-SHA512 KAT SUCCESS EXECUTING SHA224 SELF-TEST

  • SHA224 KAT SUCCESS EXECUTING SHA256 SELF-TEST

  • SHA256 KAT SUCCESS EXECUTING SHA384 SELF-TEST

  • SHA384 KAT SUCCESS EXECUTING SHA512 SELF-TEST

  • SHA512 KAT SUCCESS

END OF ELS PKC FIPS SELF-TEST