stm_match_interrupt#
Overview#
The stm driver example is to demonstrate usage of the SDK STM driver with interrupt callback functions. In this example two channels are configured with different match values, when STM timer count matches the channel value, “Channel ${number} match.” log will be printed to the terminal from interrupt callback function for this channel.
Supported Boards#
FRDM-MCXE31B
Hardware requirements
Type-C USB cable
FRDM-MCXE31B board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the terminal window:
STM match example.
Channel 1 match.
Channel 0 match.
Channel 1 match.
Channel 1 match.
Channel 0 match.
Channel 1 match.
FRDM-MCXE32B
Hardware requirements
Type-C USB cable
FRDM-MCXE32B board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the terminal window:
STM match example.
Channel 1 match.
Channel 0 match.
Channel 1 match.
Channel 1 match.
Channel 0 match.
Channel 1 match.