tempsensor#
Overview#
The TMPSNS project is a simple demonstration program of the SDK TMPSNS driver.The temperature sensor (TMPSNS) module features alarm functions that can raise independent interrupt signals if the temperature is above the high-temperature thresholds threshold, the system can then use this module to monitor the on-die temperature and take appropriate actions.
Supported Boards#
MIMXRT1170-EVKB
Hardware requirements
Mini/micro USB cable
EVK-MIMXRT1170 board
Personal Computer
Board settings
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
TMPSNS driver example.
The chip initial temperature is 23.4 ℃.
The chip temperature has reached high temperature that is 30.9 ℃.
~~~~~~~~~~~~~~~~~~~~~~~
Note 1:
To run this exmaple successfully, you should heating the chip outside, such as blowing heating.
Note 2:
To debug in qspiflash, following steps are needed:
1. Select the flash target and compile.
3. Set the SW1: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J11.
4. Start debugging in IDE.
- Keil: Click "Download (F8)" to program the image to qspiflash first then clicking "Start/Stop Debug Session (Ctrl+F5)" to start debugging.
MIMXRT1160-EVK
Hardware requirements
Mini/micro USB cable
EVK-MIMXRT1160 board
Personal Computer
Board settings
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
TMPSNS driver example.
The chip initial temperature is 23.4 ℃.
The chip temperature has reached high temperature that is 27.2 ℃.
The chip will to be waiting a desired cool down temperature .
The chip temperature has reached high temperature that is 27.2 ℃.
The chip will to be waiting a desired cool down temperature .
The chip temperature has reached high temperature that is 27.2 ℃.
The chip will to be waiting a desired cool down temperature .
......
~~~~~~~~~~~~~~~~~~~~~~~
Note 1:
To run this exmaple successfully, you should heating the chip outside, such as blowing heating.
Note 2:
To debug in qspiflash, following steps are needed:
1. Select the flash target and compile.
3. Set the SW1: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J11.
4. Start debugging in IDE.
- Keil: Click "Download (F8)" to program the image to qspiflash first then clicking "Start/Stop Debug Session (Ctrl+F5)" to start debugging.
MIMXRT1180-EVK
Hardware requirements
Mini/micro USB cable
MIMXRT1180-EVK board
Personal Computer
Board settings
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
TMPSNS driver example.
The chip initial temperature is 23.4 ℃.
The chip temperature has reached high temperature that is 30.9 ℃.
~~~~~~~~~~~~~~~~~~~~~~~
Note 1:
To run this exmaple successfully, you should heating the chip outside, such as blowing heating.
FRDM-IMXRT1186
Hardware requirements
Type-C USB cable
FRDM-IMXRT1186 board
Personal Computer
Board settings
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
TMPSNS driver example.
The chip initial temperature is 23.4 ℃.
The chip temperature has reached high temperature that is 30.9 ℃.
~~~~~~~~~~~~~~~~~~~~~~~
Note 1:
To run this exmaple successfully, you should heating the chip outside, such as blowing heating.
FRDM-IMXRT1152
Hardware requirements
Type-C USB cable
FRDM-IMXRT1152 board
Personal Computer
Board settings
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
TMPSNS driver example.
The chip initial temperature is 23.4 ℃.
The chip temperature has reached high temperature that is 30.9 ℃.
~~~~~~~~~~~~~~~~~~~~~~~
Note 1:
To run this exmaple successfully, you should heating the chip outside, such as blowing heating.
Note 2:
To debug in qspiflash, following steps are needed:
1. Select the flash target and compile.
3. Set the SW4: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J13.
4. Start debugging in IDE.
- Keil: Click "Download (F8)" to program the image to qspiflash first then clicking "Start/Stop Debug Session (Ctrl+F5)" to start debugging.