Wireless Zigbee#
The following documents provide details on how to demonstrate the capabilities of the NXP Wireless SoC when used as a Zigbee Coprocessor together with a Zigbee application running on the iMX8 (or x86) platform under Linux.
The following user guides explain how to use Bluetooth LE - Zigbee dynamic mode applications in the context of a Zigbee commissioning over Bluetooth LE use case.
The following documents are provided in PDF format. Later release may convert the pdf documentation to markdown for better review and aligned format.
For other NXP platforms that are not part of this NXP SDK delivery vehicle namely K32W061/041M/041AM/JN5189/JN5188, in order to find out more about the Zigbee related documentation, please consult the deliverables and the software offerings available at https://www.nxp.com/products/K32W061_41.