XBIC#
Overview#
The XBIC Example project is to demonstrate usage of the KSDK xbic driver. In this example, The XBIC will enable master port and slave port error detection. Then inject errors into the communication and check whether the error information is correct.
Running the demo#
When the example runs successfully, you can see the similar information from the terminal as below.
XBIC Example started !
XBIC error Injected successfully !
XBIC error data received successfully !
XBIC Example finished !
Supported Boards#
FRDM-MCXE31B
Hardware requirements
Type-C USB cable
FRDM-MCXE31B board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
XBIC Example started !
XBIC error Injected successfully !
XBIC error data received successfully !
XBIC Example finished !
FRDM-MCXE32B
Hardware requirements
Type-C USB cable
FRDM-MCXE32B board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
XBIC Example started !
XBIC error Injected successfully !
XBIC error data received successfully !
XBIC Example finished !