pdm_sai_multi_channel_tdm_edma#
Overview#
The pdm sai multi channel tdm edma example shows how to use pdm driver with edma in tdm mode:
In this example, pdm gathers eight channels’ audio data though edma, then sai sends it to codec.
Supported Boards#
MIMXRT1170-EVKB
Hardware requirements
Mini/micro USB cable
MIMXRT1170-EVKB board
Personal Computer
8-DMIC board
CS42448 audio board
Headphone
Board settings
MIMXRT1170-EVKB:
To enable external DMIC (J78), remove R2035, R2038.
To support CS42448 audio board, weld R1998, R2008, R2009, R2011, R2010, R2012, R2013, R2014, R2000, R2018, R2017, R2016, R2022
After running the demo. If output 3/4 or 7/8 has no sound,you should remove the J112.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board. 2 Insert the CS42448 audio board into J76. 3 Insert the 8-DMIC board into J78.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, if output 3/4 has no sound, remove the J112 and then you can hear the sound from microphone(8-DMIC board) and the log would be seen on the OpenSDA terminal like:
PDM SAI multi channel TDM edma example started!
User can press the key SW7 to adjust the MIC output gain, the gain value will be looped in the rang 0-15.
MIMXRT700-EVK
Hardware requirements
Micro USB cable
MIMXRT700-EVK board
Personal Computer
8CH-DMIC board
AUD-EXP-42448 audio board
Headphone
Board settings
To enable external DMIC (J7), remove R493. Connect AUD-EXP-42448 audio board to J21.
Prepare the Demo
Connect a USB cable between the host PC and the MCU-LINK USB port on the target board. 2 Insert the CS42448 audio board into J21. 3 Insert the 8-DMIC board into J7.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log would be seen on theterminal like:
PDM SAI multi channel TDM edma example started!