ecat_foe#
Overview#
This example demonstrates how to develop EtherCAT FoE(File Access over EtherCAT) example based on Slave Stack Code(SSC).
Note that the demo CAN NOT be built directly. Please see the “Prepare the Demo” section for more details.
Running the demo#
When FoE upgrade is successful, the serial port will output:
System reset...
hello sbl.
Bootloader Version 1.9.0
Primary image: magic=good, swap_type=0x1, copy_done=0x3, image_ok=0x1
Secondary image: magic=good, swap_type=0x1, copy_done=0x3, image_ok=0x3
Boot source: none
Swap type: test
Starting swap using move algorithm.
Bootloader chainload address offset: 0x40000
Reset_Handler address offset: 0x40400
Jumping to the image
Start the SSC FoE example...
Image version: 2.3.0
Image state: testing
Set image as confirmed: success
TwinCAT Setup#
To demonstrate this FoE example, TwinCAT is used as the EtherCAT MainDevice.
Supported Boards#
MIMXRT1180-EVK
Hardware requirements
MIMXRT1180-EVK RevC
RJ45 Network cable
Mini/micro USB cable
Personal Computer on which the TwinCat3 has been installed(Windows 10 is recommended)
Board settings
No special settings are required.
EEPROM LPI2C Emulator
i.MX RT1180 supports EEPROM LPI2C emulator, please skip this chapter if you used EEPROM hardware.
Hardware Setting
Connection:
J51: pin4 <–> J44: pin20
J51: pin6 <–> J44: pin18
Remove EEPROM:
U48
Add EEPROM_I2C_EMULATOR macro
Add EEPROM_I2C_EMULATOR macro to enable eeprom i2c emulator funtion
Now you can refer “Prepare the Demo” to setup ecat_examples
MCUBoot layout
Region |
From |
To |
Size |
|---|---|---|---|
MCUboot code |
0x28000000 |
0x2803FFFF |
256kB |
Primary slot |
0x28040000 |
0x2823FFFF |
2048kB |
Secondary slot |
0x28240000 |
0x2843FFFF |
2048kB |
MCUBoot header size is set to 1024 bytes
Signing algorithm is ECDSA-P256
Write alignment is 4 bytes
MCUBoot is configured to use
SWAP_MOVEimage handling strategy
Prepare the Demo
Generate the SSC source code
Download Slave Stack Code Tool(SSC Tool V5.13) from BECKHOFF official website and install it
Open Slave Stack Code Tool
Click ‘File’ -> ‘New’ -> ‘Import’ to import the Congfig file Select foe.xml under path ‘.\boards\evkmimxrt1180\ecat_examples\foe<core>\SSC’.
Click ‘Custom’ -> ‘NXP ECAT…’ -> ‘OK’ to select the subdevice description file
Click ‘Tool’ -> ‘Application’ -> ‘Import’ to import Application information Select foe.xlsx under path ‘.\boards\evkmimxrt1180\ecat_examples\foe<core>\SSC’.
Click ‘Project’ -> ‘Create new Slave Files’ ‘Source Folder’(default): ‘.\boards\evkmimxrt1180\ecat_examples\foe<core>\SSC\Src’. Click ‘Start’.
Remove foe.c under Src folder
Connect EtherCAT Port0 with TwinCAT3
RJ45 interface labeled as J28 is the EtherCAT Port0 and RJ45 interface labeled as J32 is the EtherCAT Port1.
Connect a USB cable between the host PC and the OpenSDA USB port on the target board
Open a serial terminal with the following settings
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Compile mcuboot_opensource and FoE example image
mcuboot_opensource example path: ‘boards\evkmimxrt1180\ota_examples\mcuboot_opensource\cm33’
FoE example path: ‘boards\evkmimxrt1180\ecat_examples\foe\cm33’
Download mcuboot_opensource and signed FoE image to the target board using ‘MCUXpresso Secure Provisioning Tool’
Download ‘MCUXpresso Secure Provisioning Tool’ from NXP official website
Change EVK SW5[1..4] to 0000 and press the reset SW3 key
Open ‘SPT’ and create a new workspace for the selected processor
Connect the board via UART
Verify the selected boot memory in ‘main menu’ > ‘Target’ > ‘Boot Memory’
On the Build image view, select the ‘mcuboot_opensource_cm33.elf’ image as ‘Source executable image’
Open ‘main menu’ > ‘Tools’ > ‘MCUboot’ > ‘Sign Image’ and configure the following
‘ecat_foe.bin’ image to be signed
The signing key; it is located in the same folder that the prebuilt application or in MCUXpresso SDK, in folder ‘middleware\mcuboot_opensource\boot\nxp_mcux_sdk\keys\sign-ecdsa-p256-priv.pem’
The imgtool arguments by default should match the SDK example. It is not needed to change them
Click the ‘Sign’ button to sign the application; fix problems, if any
Set target address: ‘0x28040000’
Close the dialog by clicking the ‘Save & Close’ button
On the Build tab, double-check that the ‘Build script hooks’ section contains the pre-build script
Open ‘Additional Images’ and check that the signed application is properly configured as ‘Image 1’
Build and write the bootable image into the processor
Note: You can refer ‘MCUboot workflow’ chapter of ‘MCUXSPTUG.pdf’, which is from ‘SPT Documentation page’
Run FoE example
Change EVK SW5[1..4] to 0100 and press the reset SW3 key.
The serial port will output:
hello sbl. Bootloader Version 1.9.0 Primary image: magic=good, swap_type=0x1, copy_done=0x3, image_ok=0x1 Secondary image: magic=unset, swap_type=0x1, copy_done=0x3, image_ok=0x3 Boot source: primary slot Swap type: none Bootloader chainload address offset: 0x40000 Reset_Handler address offset: 0x40400 Jumping to the image Start the SSC FoE example... Image version: 2.3.0
Update ESI file to EEPROM
Copy ESI file ‘ECAT-FOE.xml’ generated by SSC TOOL to <TwinCAT_installation_folder>/<twincat_version>/Config/io/EtherCAT/
Restart TwinCAT3 IDE
Scan device and Update EEPROM
Scan and load this device and create a PLC project in TwinCat3
The PLC Main code is as follows:
PROGRAM MAIN VAR Delay : TON; LedIn AT %I* : BOOL; LedOut AT %Q* : BOOL; END_VAR Delay(IN := TRUE, PT := T#1S); IF Delay.Q THEN LedOut := NOT LedIn; Delay(IN := FALSE); END_IF;
Activate configuration
Click ‘TwinCAT’ -> ‘Restart TwinCAT(Config Mode)’ to activate configuration
FoE image upgrade
Compile FoE image
Install imgtool by the Python package manager
‘pip install imgtool’
Generate new version FoE example signed image
‘imgtool sign –key sign-ecdsa-p256-priv.pem –align 4 –header-size 0x400 –pad-header –slot-size 0x200000 –max-sectors 800 –version “2.4.0” ecat_foe.bin ecat_foe_2-4-0_SIGNED.bin’
Click ‘Device’ -> ‘Box1’ -> ‘Online’ -> ‘Bootstrap’
Click ‘Download’ -> ‘ecat_foe_2-4-0_SIGNED.bin’ -> ‘Password: 12369874’ -> ‘Ok’ to upgrade image
The serial port will output:
Firmware upgrade in progress... FoE_StoreImage: processed 116 bytes FoE_StoreImage: processed 232 bytes ... FoE_StoreImage: upload complete (42028 bytes) write magic number offset = 0x43ff00 Update image success
After download, click ‘Init’ to restart board
FoE image download
Click ‘Upload’ -> ‘ecat_foe_2-4-0_SIGNED.bin’ -> ‘Ok’ to download upgraded image
Note:
For subsequent upgrades, new version number must be greater than the old version number, perform step 11 to generate the new version signed image
For more mcuboot information, please refer to mcuboot_opensource example
FRDM-MIMXRT1186
Hardware requirements
FRDM-IMXRT1186 A2
RJ45 Network cable
Type-C USB cable
Personal Computer on which the TwinCat3 has been installed(Windows 10 is recommended)
Board settings
J12(2-3)/J13(2-3): eCAT0 Function Via J57A(Default).
J18(2-3)/J17(2-3): eCAT1 Function Via J57B(Default).
MCUBoot layout
Region |
From |
To |
Size |
|---|---|---|---|
MCUboot code |
0x04000000 |
0x0403FFFF |
256kB |
Primary slot |
0x04040000 |
0x0423FFFF |
2048kB |
Secondary slot |
0x04240000 |
0x0443FFFF |
2048kB |
MCUBoot header size is set to 1024 bytes
Signing algorithm is ECDSA-P256
Write alignment is 4 bytes
MCUBoot is configured to use
SWAP_MOVEimage handling strategy
EEPROM LPI2C Emulator
FRDM-IMXRT1186 supports EEPROM LPI2C emulator, please skip this chapter if you used EEPROM hardware.
Hardware Setting
Remove Jumper:
J31: pin1 - pin2
J35: pin1 - pin2
Remove Resistors:
R297: pin1 - pin2
R299: pin1 - pin2
Add Resistors:
R30
R31
R297: pin1 - pin3
R299: pin1 - pin3
Connection:
J31: pin1 <–> J2: pin18
J35: pin1 <–> J2: pin20
Add EEPROM_I2C_EMULATOR macro
Add EEPROM_I2C_EMULATOR macro to enable eeprom i2c emulator funtion
Now you can refer “Prepare the Demo” to setup ecat_examples
Prepare the Demo
Generate the SSC source code
Download Slave Stack Code Tool(SSC Tool V5.13) from BECKHOFF official website and install it
Open Slave Stack Code Tool
Click ‘File’ -> ‘New’ -> ‘Import’ to import the Congfig file Select foe.xml under path ‘.\boards\frdmimxrt1186\ecat_examples\foe<core>\SSC’.
Click ‘Custom’ -> ‘NXP ECAT…’ -> ‘OK’ to select the subdevice description file
Click ‘Tool’ -> ‘Application’ -> ‘Import’ to import Application information Select foe.xlsx under path ‘.\boards\frdmimxrt1186\ecat_examples\foe<core>\SSC’.
Click ‘Project’ -> ‘Create new Slave Files’ ‘Source Folder’(default): ‘.\boards\frdmimxrt1186\ecat_examples\foe<core>\SSC\Src’. Click ‘Start’.
Remove foe.c under Src folder
Connect EtherCAT Port0 with TwinCAT3
RJ45 interface labeled as J57A is the EtherCAT Port0 and RJ45 interface labeled as J57B is the EtherCAT Port1.
Connect a USB cable between the host PC and the OpenSDA USB port on the target board
Open a serial terminal with the following settings
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Compile mcuboot_opensource and FoE example image
mcuboot_opensource example path: ‘boards\frdmimxrt1186\ota_examples\mcuboot_opensource\cm33’
FoE example path: ‘boards\frdmimxrt1186\ecat_examples\foe\cm33’
Download mcuboot_opensource and signed FoE image to the target board using ‘MCUXpresso Secure Provisioning Tool’
Download ‘MCUXpresso Secure Provisioning Tool’ from NXP official website
Change J60(from left to right)[1,2,3] to ‘100’ to open Serial Download mode, reset board
Open ‘SPT’ and create a new workspace for the selected processor
Connect the board via UART
Verify the selected boot memory in ‘main menu’ > ‘Target’ > ‘Boot Memory’
On the Build image view, select the ‘mcuboot_opensource_cm33.elf’ image as ‘Source executable image’
Open ‘main menu’ > ‘Tools’ > ‘MCUboot’ > ‘Sign Image’ and configure the following
‘ecat_foe.bin’ image to be signed
The signing key; it is located in the same folder that the prebuilt application or in MCUXpresso SDK, in folder ‘middleware\mcuboot_opensource\boot\nxp_mcux_sdk\keys\sign-ecdsa-p256-priv.pem’
The imgtool arguments by default should match the SDK example. It is not needed to change them
Click the ‘Sign’ button to sign the application; fix problems, if any
Set target address: ‘0x04040000’
Close the dialog by clicking the ‘Save & Close’ button
On the Build tab, double-check that the ‘Build script hooks’ section contains the pre-build script
Open ‘Additional Images’ and check that the signed application is properly configured as ‘Image 1’
Build and write the bootable image into the processor
Note: You can refer ‘MCUboot workflow’ chapter of ‘MCUXSPTUG.pdf’, which is from ‘SPT Documentation website page’
Run FoE example
Change J60(from left to right)[1,2,3] to ‘001’, reset board
The serial port will output:
hello sbl. Bootloader Version 1.9.0 Primary image: magic=good, swap_type=0x1, copy_done=0x3, image_ok=0x1 Secondary image: magic=unset, swap_type=0x1, copy_done=0x3, image_ok=0x3 Boot source: primary slot Swap type: none Bootloader chainload address offset: 0x40000 Reset_Handler address offset: 0x40400 Jumping to the image
Start the SSC FoE example… Image version: 2.3.0
Update ESI file to EEPROM
Copy ESI file ‘ECAT-FOE.xml’ generated by SSC TOOL to <TwinCAT_installation_folder>/<twincat_version>/Config/io/EtherCAT/
Restart TwinCAT3 IDE
Scan device and Update EEPROM
Scan and load this device and create a PLC project in TwinCat3
The PLC Main code is as follows:
PROGRAM MAIN VAR Delay : TON; LedIn AT %I* : BOOL; LedOut AT %Q* : BOOL; END_VAR Delay(IN := TRUE, PT := T#1S); IF Delay.Q THEN LedOut := NOT LedIn; Delay(IN := FALSE); END_IF;
Activate configuration
Click ‘TwinCAT’ -> ‘Restart TwinCAT(Config Mode)’ to activate configuration
FoE image upgrade
Generate new version FoE example signed image ‘imgtool sign –key sign-ecdsa-p256-priv.pem –align 4 –header-size 0x400 –pad-header –slot-size 0x200000 –max-sectors 800 –version “2.4.0” ecat_foe_cm33.bin ecat_foe_2-4-0_SIGNED.bin’
Click ‘Device’ -> ‘Box1’ -> ‘Online’ -> ‘Bootstrap’
Click ‘Download’ -> ‘ecat_foe_2-4-0_SIGNED.bin’ -> ‘Password: 12369874’ -> ‘Ok’ to upgrade image
The serial port will output:
Firmware upgrade in progress... FoE_StoreImage: processed 116 bytes FoE_StoreImage: processed 232 bytes ... FoE_StoreImage: upload complete (42028 bytes) write magic number offset = 0x43ff00 Update image success
After download, click ‘Init’ to restart board
FoE image download
Click ‘Upload’ -> ‘ecat_foe_2-4-0_SIGNED.bin’ -> ‘Ok’ to download upgraded image
Note:
- For subsequent upgrades, new version number must be greater than the old version number, perform step 11 to generate the new version signed image
- For more mcuboot information, please refer to mcuboot_opensource example