MCUXpresso SDK Documentation

USB_DeviceGetHidDescriptor

USB_DeviceGetHidDescriptor#

/* Get HID descriptor request */
usb_status_t USB_DeviceGetHidDescriptor(usb_device_handle handle,
                                         usb_device_get_hid_descriptor_struct_t *hidDescriptor)
{
    /* If this request is not supported, return the error code “kStatus_USB_InvalidRequest”. Otherwise, fill the hidDescriptor with the descriptor buffer address and length based on the interface number. */
    return kStatus_USB_InvalidRequest;
}

Parent topic:USB descriptor functions

Parent topic:USB composite device descriptor examples