MCUXpresso SDK Documentation

decnano_decompress

decnano_decompress#

Overview#

The DECNano decompress Demo reads the RGB888 or ARGB8888 picture that is compressed in DECNano format, decompress them, and shows them in the LCD panel. Change the DEMO_PIC_FORMAT in input.h to test other compressed formats, all 6 DECNano compressed formats are supported. Note this example demonstrates the LCDIF controller function, so only DEMO_PANEL_RK055AHD091, DEMO_PANEL_RK055IQH091, DEMO_PANEL_RK055MHD091 and DEMO_PANEL_RASPI_7INCH are supported.

Supported Boards#