tflm_cifar10#
Overview#
Convolutional neural network (CNN) example with the use of convolution, ReLU activation, pooling and fully-connected functions.
The CNN model in the example was trained using the scripts available at [1] with the CifarNet model. The configuration of the model was modified to match the neural network structure in the CMSIS-NN CIFAR-10 example. The example source code is a modified version of the Label Image example from the TensorFlow Lite examples [2], adjusted to run on MCUs. The neural network consists of 3 convolution layers interspersed by ReLU activation and max pooling layers, followed by a fully-connected layer at the end. The input to the network is a 32x32 pixel color image, which is classified into one of the 10 output classes. The model size is 91 KB.
Firstly a static ship image is used as input regardless camera is connected or not. Secondly runtime image processing from camera in the case camera and display is connected. Camera data are displayed on LCD.
HOW TO USE THE APPLICATION: To classify an image, place an image in front of the camera so that it fits in the white rectangle in the middle of the LCD display. Note that semihosting implementation causes slower or discontinuous video experience. Select UART in ‘Project Options’ during project import for using external debug console via UART (virtual COM port).
[1] https://github.com/tensorflow/models/tree/master/research/slim [2] https://github.com/tensorflow/tensorflow/tree/r2.3/tensorflow/lite/examples/label_image
Files: main.cpp - example main function ship.bmp - shrinked picture of the object to recognize (source: https://en.wikipedia.org/wiki/File:Christian_Radich_aft_foto_Ulrich_Grun.jpg) image_data.h - image file converted to a C language array of RGB values using Python with the OpenCV and Numpy packages: import cv2 import numpy as np img = cv2.imread(‘ship.bmp’) img = cv2.cvtColor(img, cv2.COLOR_BGR2RGB) with open(‘image_data.h’, ‘w’) as fout: print(‘#define STATIC_IMAGE_NAME “ship”’, file=fout) print(‘static const uint8_t image_data[] = {’, file=fout) img.tofile(fout, ‘, ‘, ‘0x%02X’) print(‘};\n’, file=fout) timer.c - timer source code image/* - image capture and pre-processing code model/get_top_n.cpp - top results retrieval model/model_data.h - model data converted from a .tflite file to a C language array using the xxd tool (distributed with the Vim editor at www.vim.org) model/model.cpp - model initialization and inference code model/model_cifarnet_ops.cpp - model operations registration model/output_postproc.cpp - model output processing video/* - camera and display handling
Running the demo#
The log below shows the output of the demo in the terminal window (compiled with ARM GCC):
Starting HiFi4 example from Cortex-M33 core DSP Init Susccessfully CIFAR-10 example using a TensorFlow Lite Micro model. Detection threshold: 60% Model: cifarnet_quant_int8_npu Hifi4 DSP Frequency: 324 MHz TensorArena Addr: 0x204697e0 - 0x204777e0 TensorArena Size: Total 0xe000 (57344 B); Used 0xaee8 (44776 B) Model Addr: 0x20400980 - 0x20418d60 Model Size: 0x183e0 (99296 B) Total Size Used: 144072 B (Model (99296 B) + TensorArena (44776 B))
Static data processing:#
Inference time: 1014 us
Detected: ship (99%)
Supported Boards#
[MIMXRT700-EVK]