MCUXpresso SDK Documentation

ele_derive_key#

Overview#

The ELE derive key application provides example how to use SSSAPI to derive keys by utilising the HKDF functionality, as well as how to derive keys for an Elliptic Curve Diffie-Hellman key exchange operation.

Warning#

Please note that HKDF flow depends on the revision of your chip. Expected inputs for various steps of HKDF have changed with chip revision A2.1. Below is a brief overview of the two variants.

The change relates only to the HKDF Extract step.

For revisions A0 through A2:#

When initializing a key derivation context for any variant of kAlgorithm_SSS_HKDF_*_EXTRACT via sss_sscp_derive_key_context_init(), salt is to be passed as a key object. Next, when calling sss_sscp_derive_key() for the Extract step, the Input Keying Material (IKM) is passed as an input buffer.

For revision A2.1:#

The order and approach to passing salt and IKM are swapped compared to previous revisions.

When initializing a key derivation context for any variant of kAlgorithm_SSS_HKDF_*_EXTRACT via sss_sscp_derive_key_context_init(), IKM is to be passed as a key object. Next, when calling sss_sscp_derive_key() for the Extract step, the salt is passed as an input buffer.

This approach allows for keeping the IKM opaque (e.g. taking IKM from the result of an ECDH or SPAKE2+ operation).

Note#

By default, IAR’s “Static clustering” optimization option is enabled in the IAR release targets. Compile flag --no_clustering has been added to the build to disable static clustering due to it causing erroneous execution of this example.

Running the demo#

The following lines are printed to the serial terminal when the demo program is executed. The output shown is the output of the example with chip revision A2.1.

ELE Derive Key via SSSAPI Example

**** Elliptic Curve Diffie-Hellman ****
Init Alice key object...OK
Init Bob key object...OK
Init shared key object...OK
Allocate Alice key object handle...OK
Allocate Bob key object handle...OK
Allocate shared key object handle...OK
Initialize RNG before key generation...OK
Import Alice key pair...OK
Import Bob public key...OK
Init Derive Key Context...OK
ECDH key derivation...OK
Get derived shared secret...OK
Derived shared secret matches expected shared secret...OK
Cleanup...OK

**** HDKF key derivation ****
Init IKM key object...OK
Init PRK key object...OK
Init OKM key object...OK
Allocate IKM key handle...OK
Allocate PRK key handle...OK
Allocate OKM key handle...OK
Set IKM...OK
Initialize HKDF SHA256 extract step context...OK
HKDF SHA256 extract...OK
Free HKDF SHA256 extract step context...OK
Initialize HKDF SHA256 expand step context...OK
HKDF SHA256 expand...OK
Get OKM...OK
Derived OKM matches expected OKM...OK
Cleanup...OK

End of Example with SUCCESS!!

Example end

Supported Boards#

KW47-EVK
Hardware requirements
  • Type-C USB cable

  • KW47-EVK Board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board J14.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

MCX-W72-EVK
Hardware requirements
  • Type-C USB cable

  • MCX-W72-EVK Board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board J14.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

KW47-LOC
Hardware requirements
  • Type-C USB cable

  • KW47-LOC Board

  • Personal Computer

Board settings

No special is needed.

Prepare the Demo
  1. Connect a USB cable between the host PC and the LOC board J3.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

MCXW72-LOC
Hardware requirements
  • Type-C USB cable

  • MCXW72-LOC Board

  • Personal Computer

Board settings

No special is needed.

Prepare the Demo
  1. Connect a USB cable between the host PC and the LOC board J3.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXW72
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXW72 Board

  • Personal Computer

Board settings

No special is needed.

Prepare the Demo
  1. Connect a USB cable between the host PC and the FRDM board J10.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.