puf_1#
Overview#
The PUF Example project is a demonstration program that uses the KSDK software implement secure key storage using PUF software driver.
Usual use consists of these steps:
Start: The Activation Code (AC) generated during the enroll operation and the Startup Data (SD) are used to reconstruct the digital fingerprint. It is done after every power-up and reset.
Generate Key: The controller generates an unique key and combines it with the digital fingerprint to output a key code. Each time a Generate Key operation is executed a new unique key is generated.
Set Key: The digital fingerprint generated during the Enroll/Start operations and the key provided by the Client Design (CD) are used to generate a Key Code (KC). This KC can be stored externally. Perform this operation only once for each key.
Get Key: The digital fingerprint generated during the Start operation and the KC generated during a Set Key operation are used to retrieve a stored key. Perform this operation every time a key is needed.