MCUXpresso SDK Documentation

flexio_pwm

flexio_pwm#

Overview#

This demo describes how to use SDK drivers to implement the PWM feature by FLEXIO IP module. It outputs the PWM singal with fixed frequency defined by “DEMO_FLEXIO_FREQUENCY” in source code and dynamic duty from 99 to 1 to one of the FLEXIO pins.

Supported Boards#

IMX943-EVK
Hardware requirements
  • Micro USB cable

  • IMX943-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

Connect J43-12 to Oscilloscope or Logic Analyzer.

Please note this application can’t support running with Linux BSP!
Note

Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.

Prepare the Demo
  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW1(SYS_PWR) to power on the board.

  2. Connect a micro USB cable between the host PC and the J15(FTDI_DEBUG) USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either re-power up your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, if the input duty cycle range is 0~100, the trigger signal can be captured on OSC. You can see similar information from the terminal as follows:

FLEXIO_PWM demo start.

Please input a value (0 - 100) to set duty cycle: 10
Input value is 10

PWM duty cycle is: 10

PWM leave is: 0

Please input a value (0 - 100) to set duty cycle: 150
Input value is 150
Your value is output of range.
Set pwm output to IDLE.

Please input pwm idle status (0 or 1): 1
Input IDLE state value is 1

PWM leave is: 1

Please input a value (0 - 100) to set duty cycle:
......

Note:

  1. The duty cycle of the PWM is variable, except for the idle state, 0 and 100.

  2. If the input duty cycle range exceeds 100, the pwm will be set to idle state

  3. If the set pwm idle value is out of range, it will output “Your value is output of range.” and then return to set the duty cycle.