MCUXpresso SDK Documentation

USB descriptor functions#

All USB device descriptor and functions are placed in the “usb_device_descriptor.c” file.

USB descriptor#

The descriptors for each class can be obtained from the class-related examples and class specification. For the composite device, combine multiple class descriptors.

Note: The interface number in the configuration descriptor must be the correct interface number value. The endpoint number value in each endpoint descriptor must be consistent with the structures in usb_device_endpoint_struct_t.

Parent topic:USB descriptor functions

USB_DeviceGetDeviceDescriptor#

This function is used to get the device descriptor. All devices must implement this function.

usb_status_t USB_DeviceGetDeviceDescriptor(usb_device_handle handle,
                                           usb_device_get_device_descriptor_struct_t *deviceDescriptor)
{
    deviceDescriptor->buffer = g_UsbDeviceDescriptor;
    deviceDescriptor->length = USB_DESCRIPTOR_LENGTH_DEVICE;
    return kStatus_USB_Success;
}

Parent topic:USB descriptor functions

Parent topic:USB composite device descriptor examples

USB_DeviceGetConfigurationDescriptor#

This function is used to get the configuration descriptor. All devices must implement this function.

/* Get device configuration descriptor request */
usb_status_t USB_DeviceGetConfigurationDescriptor(
    usb_device_handle handle, usb_device_get_configuration_descriptor_struct_t *configurationDescriptor)
{
    if (USB_COMPOSITE_CONFIGURE_INDEX > configurationDescriptor->configuration)
    {
        configurationDescriptor->buffer = g_UsbDeviceConfigurationDescriptor;
        configurationDescriptor->length = USB_DESCRIPTOR_LENGTH_CONFIGURATION_ALL;
        return kStatus_USB_Success;
    }
    return kStatus_USB_InvalidRequest;
}

Parent topic:USB descriptor functions

Parent topic:USB composite device descriptor examples

USB_DeviceGetStringDescriptor#

This function is used to get the string descriptor. All devices must implement this function.


/* Get device string descriptor request */
usb_status_t USB_DeviceGetStringDescriptor(usb_device_handle handle,
                                            usb_device_get_string_descriptor_struct_t *stringDescriptor)
{
    if (stringDescriptor->stringIndex == 0U)
    {
        stringDescriptor->buffer = (uint8_t *)g_UsbDeviceLanguageList.languageString;
        stringDescriptor->length = g_UsbDeviceLanguageList.stringLength;
    }
    else
    {
        uint8_t languageId = 0U;
        uint8_t languageIndex = USB_DEVICE_STRING_COUNT;
        for (; languageId < USB_DEVICE_STRING_COUNT; languageId++)
        {
            if (stringDescriptor->languageId == g_UsbDeviceLanguageList.languageList[languageId].languageId)
            {
                if (stringDescriptor->stringIndex < USB_DEVICE_STRING_COUNT)
                {
                    languageIndex = stringDescriptor->stringIndex;
                }
                break;
            }
        }
        if (USB_DEVICE_STRING_COUNT == languageIndex)
        {
            return kStatus_USB_InvalidRequest;
        }
        stringDescriptor->buffer = (uint8_t *)g_UsbDeviceLanguageList.languageList[languageId].string[languageIndex];
        stringDescriptor->length = g_UsbDeviceLanguageList.languageList[languageId].length[languageIndex];
    }
    return kStatus_USB_Success;
}

Parent topic:USB descriptor functions

Parent topic:USB composite device descriptor examples

USB_DeviceGetHidDescriptor#

/* Get HID descriptor request */
usb_status_t USB_DeviceGetHidDescriptor(usb_device_handle handle,
                                         usb_device_get_hid_descriptor_struct_t *hidDescriptor)
{
    /* If this request is not supported, return the error code “kStatus_USB_InvalidRequest”. Otherwise, fill the hidDescriptor with the descriptor buffer address and length based on the interface number. */
    return kStatus_USB_InvalidRequest;
}

Parent topic:USB descriptor functions

Parent topic:USB composite device descriptor examples

USB_DeviceGetHidReportDescriptor#

/* Get the HID report descriptor request */
usb_status_t USB_DeviceGetHidReportDescriptor(usb_device_handle handle,
                                                usb_device_get_hid_report_descriptor_struct_t *hidReportDescriptor)
{
    if (USB_HID_GENERIC_INTERFACE_INDEX == hidReportDescriptor->interfaceNumber)
    {
        hidReportDescriptor->buffer = g_UsbDeviceHidGenericReportDescriptor;
        hidReportDescriptor->length = USB_DESCRIPTOR_LENGTH_HID_GENERIC_REPORT;
    }
    else if (USB_HID_KEYBOARD_INTERFACE_INDEX == hidReportDescriptor->interfaceNumber)
    {
        hidReportDescriptor->buffer = g_UsbDeviceHidKeyboardReportDescriptor;
        hidReportDescriptor->length = USB_DESCRIPTOR_LENGTH_HID_KEYBOARD_REPORT;
    }
    else
    {
        return kStatus_USB_InvalidRequest;
    }
    return kStatus_USB_Success;
}

Parent topic:USB descriptor functions

Parent topic:USB composite device descriptor examples

USB_DeviceGetHidPhysicalDescriptor#

/* Get the HID physical descriptor request */
usb_status_t USB_DeviceGetHidPhysicalDescriptor(
    usb_device_handle handle, usb_device_get_hid_physical_descriptor_struct_t *hidPhysicalDescriptor)
{
    /* If this request is not supported, return the error code “kStatus_USB_InvalidRequest”. Otherwise, fill the hidPhysicalDescriptor with the descriptor buffer address and length based on the interface number and the physical index. */
    return kStatus_USB_InvalidRequest;
}

Parent topic:USB descriptor functions

Parent topic:USB composite device descriptor examples

USB_DeviceSetSpeed#

/* Because HS and FS descriptors are different, update the device descriptors and configurations to match the current speed.
 * By default, the device descriptors and configurations are configured by using FS parameters for both EHCI and KHCI.
 * When the EHCI is enabled, the application needs to call this function to update the device by using current speed.
 * The updated information includes the endpoint max packet size, endpoint interval, and so on. */
usb_status_t USB_DeviceSetSpeed(usb_device_handle handle, uint8_t speed)
{
    usb_descriptor_union_t *descriptorHead;
    usb_descriptor_union_t *descriptorTail;
    descriptorHead = (usb_descriptor_union_t *)&g_UsbDeviceConfigurationDescriptor[0];
    descriptorTail = (usb_descriptor_union_t *)(&g_UsbDeviceConfigurationDescriptor[USB_DESCRIPTOR_LENGTH_CONFIGURATION_ALL - 1U]);
    while (descriptorHead < descriptorTail)
    {
        if (descriptorHead->common.bDescriptorType == USB_DESCRIPTOR_TYPE_ENDPOINT)
        {
            if (USB_SPEED_HIGH == speed)
            {
                if (USB_HID_KEYBOARD_ENDPOINT_IN == (descriptorHead->endpoint.bEndpointAddress & USB_ENDPOINT_NUMBER_MASK))
                {
                    descriptorHead->endpoint.bInterval = HS_HID_KEYBOARD_INTERRUPT_IN_INTERVAL;
                    USB_SHORT_TO_LITTLE_ENDIAN_ADDRESS(HS_HID_KEYBOARD_INTERRUPT_IN_PACKET_SIZE,
                                                       descriptorHead->endpoint.wMaxPacketSize);
                }
                else if (((descriptorHead->endpoint.bEndpointAddress & USB_DESCRIPTOR_ENDPOINT_ADDRESS_DIRECTION_IN) ==
                          USB_DESCRIPTOR_ENDPOINT_ADDRESS_DIRECTION_IN) &&
                         (USB_HID_GENERIC_ENDPOINT_IN == (descriptorHead->endpoint.bEndpointAddress & USB_ENDPOINT_NUMBER_MASK)))
                {
                    descriptorHead->endpoint.bInterval = HS_HID_GENERIC_INTERRUPT_IN_INTERVAL;
                    USB_SHORT_TO_LITTLE_ENDIAN_ADDRESS(HS_HID_GENERIC_INTERRUPT_IN_PACKET_SIZE,
                                                       descriptorHead->endpoint.wMaxPacketSize);
                }
                else if (((descriptorHead->endpoint.bEndpointAddress & USB_DESCRIPTOR_ENDPOINT_ADDRESS_DIRECTION_OUT) ==
                          USB_DESCRIPTOR_ENDPOINT_ADDRESS_DIRECTION_OUT) &&
                         (USB_HID_GENERIC_ENDPOINT_OUT == (descriptorHead->endpoint.bEndpointAddress & USB_ENDPOINT_NUMBER_MASK)))
                {
                    descriptorHead->endpoint.bInterval = HS_HID_GENERIC_INTERRUPT_OUT_INTERVAL;
                    USB_SHORT_TO_LITTLE_ENDIAN_ADDRESS(HS_HID_GENERIC_INTERRUPT_OUT_PACKET_SIZE,
                                                       descriptorHead->endpoint.wMaxPacketSize);
                }
            }
            else
            {
                if (USB_HID_KEYBOARD_ENDPOINT_IN == (descriptorHead->endpoint.bEndpointAddress & USB_ENDPOINT_NUMBER_MASK))
                {
                    descriptorHead->endpoint.bInterval = FS_HID_KEYBOARD_INTERRUPT_IN_INTERVAL;
                    USB_SHORT_TO_LITTLE_ENDIAN_ADDRESS(FS_HID_KEYBOARD_INTERRUPT_IN_PACKET_SIZE,
                                                       descriptorHead->endpoint.wMaxPacketSize);
                }
                else if (((descriptorHead->endpoint.bEndpointAddress & USB_DESCRIPTOR_ENDPOINT_ADDRESS_DIRECTION_IN) ==
                          USB_DESCRIPTOR_ENDPOINT_ADDRESS_DIRECTION_IN) &&
                         (USB_HID_GENERIC_ENDPOINT_IN == (descriptorHead->endpoint.bEndpointAddress & USB_ENDPOINT_NUMBER_MASK)))
                {
                    descriptorHead->endpoint.bInterval = FS_HID_GENERIC_INTERRUPT_IN_INTERVAL;
                    USB_SHORT_TO_LITTLE_ENDIAN_ADDRESS(FS_HID_GENERIC_INTERRUPT_IN_PACKET_SIZE,
                                                       descriptorHead->endpoint.wMaxPacketSize);
                }
                else if (((descriptorHead->endpoint.bEndpointAddress & USB_DESCRIPTOR_ENDPOINT_ADDRESS_DIRECTION_OUT) ==
                          USB_DESCRIPTOR_ENDPOINT_ADDRESS_DIRECTION_OUT) &&
                         (USB_HID_GENERIC_ENDPOINT_OUT == (descriptorHead->endpoint.bEndpointAddress & USB_ENDPOINT_NUMBER_MASK)))
                {
                    descriptorHead->endpoint.bInterval = FS_HID_GENERIC_INTERRUPT_OUT_INTERVAL;
                    USB_SHORT_TO_LITTLE_ENDIAN_ADDRESS(FS_HID_GENERIC_INTERRUPT_OUT_PACKET_SIZE,
                                                       descriptorHead->endpoint.wMaxPacketSize);
                }
            }
        }
        descriptorHead = (usb_descriptor_union_t *)((uint8_t *)descriptorHead + descriptorHead->common.bLength);
    }
    for (int i = 0U; i < USB_HID_GENERIC_ENDPOINT_COUNT; i++)
    {
        if (USB_SPEED_HIGH == speed)
        {
            if (g_UsbDeviceHidGenericEndpoints[i].endpointAddress & USB_DESCRIPTOR_ENDPOINT_ADDRESS_DIRECTION_IN)
            {
                g_UsbDeviceHidGenericEndpoints[i].maxPacketSize = HS_HID_GENERIC_INTERRUPT_IN_PACKET_SIZE;
            }
            else
            {
                g_UsbDeviceHidGenericEndpoints[i].maxPacketSize = HS_HID_GENERIC_INTERRUPT_OUT_PACKET_SIZE;
            }
        }
        else
        {
            if (g_UsbDeviceHidGenericEndpoints[i].endpointAddress & USB_DESCRIPTOR_ENDPOINT_ADDRESS_DIRECTION_IN)
            {
                g_UsbDeviceHidGenericEndpoints[i].maxPacketSize = HS_HID_GENERIC_INTERRUPT_OUT_PACKET_SIZE;
            }
            else
            {
                g_UsbDeviceHidGenericEndpoints[i].maxPacketSize = FS_HID_GENERIC_INTERRUPT_OUT_PACKET_SIZE;
            }
        }
    }
    if (USB_SPEED_HIGH == speed)
    {
        g_UsbDeviceHidKeyboardEndpoints[0].maxPacketSize = HS_HID_KEYBOARD_INTERRUPT_IN_PACKET_SIZE;
    }
    else
    {
        g_UsbDeviceHidKeyboardEndpoints[0].maxPacketSize = FS_HID_KEYBOARD_INTERRUPT_IN_PACKET_SIZE;
    }
    return kStatus_USB_Success;
}

Parent topic:USB descriptor functions

Parent topic:USB composite device descriptor examples