MCUXpresso SDK Documentation

netc_txrx_transfer

netc_txrx_transfer#

Overview#

The NETC Tx/Rx transfer demo application demonstrates how to set up NETC frame transmission. In this demo, NETC PSI sends/receives frames with external loopback cable. Use MISX to handle interrupts in the transmission.

Supported Boards#

IMX943-EVK
Hardware requirements
  • Mini/micro USB cable

  • imx943evk board

  • Personal Computer

Board settings

Connect J43-12 to oscilloscope to capture the trigger signal.

Prepare the Demo
  1. Connect a USB cable between the host PC and the USB DBG port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Program flash.bin to boot source and start the board.

  4. Link up the swp2 phy.

Running the demo

When the demo runs successfully, can get timer FIPER signal on OSC.