sgi_symmetric#
Overview#
The SGI PKC application provides examples which demonstrate usage of most available algorithms and a crypto library lightweight testing:
AES-128 encryption/decryption, modes ECB/CBC/CTR/GCM/CMAC
SHA2-224/256/384/512 (including sha-direct mode)
ECC Sign/Verify/Keygen/Keyexchange
Supported Boards#
FRDM-MCXA266
Hardware requirements
Type-C USB cable
FRDM-MCXA266 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
SGI symmetric cipher example
============================
AES128-CBC oneshot encryption:pass
AES128-ECB multipart encryption:pass
CMAC AES128:pass
============================
RESULT: All 3 test PASS!!
SGI example END
FRDM-MCXA366
Hardware requirements
Type-C USB cable
FRDM-MCXA366 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
SGI symmetric cipher example
============================
AES128-CBC oneshot encryption:pass
AES128-ECB multipart encryption:pass
CMAC AES128:pass
============================
RESULT: All 3 test PASS!!
SGI example END
FRDM-MCXL255
Hardware requirements
Type-C USB cable
FRDM-MCXL255 board
Personal Computer
Board settings
Prepare the Demo
Connect a USB cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
SGI symmetric cipher example
============================
AES128-CBC oneshot encryption:pass
AES128-ECB multipart encryption:pass
CMAC AES128:pass
============================
RESULT: All 3 test PASS!!
SGI example END
FRDM-MCXA577
Hardware requirements
Type-C USB cable
FRDM-MCXA577 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
SGI symmetric cipher example
============================
AES128-CBC oneshot encryption:pass
AES128-ECB multipart encryption:pass
CMAC AES128:pass
============================
RESULT: All 3 test PASS!!
SGI example END
FRDM-KW43
Hardware requirements
Type-C USB cable
FRDM-KW43 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
SGI symmetric cipher example
============================
AES128-CBC oneshot encryption:pass
AES128-ECB multipart encryption:pass
CMAC AES128:pass
============================
RESULT: All 3 test PASS!!
SGI example END