MCUXpresso SDK Documentation

Introduction

Introduction#

This document describes the Command Line Interface (CLI) options provided with the 812.15.4 Connectivity Test application. The application provides tests for measuring transmission between two or more devices. This document also provides the test description, configuration, setup, and steps to perform the test using the application.