usb_device_interface_struct_t
This structure provides information about each alternate setting interface for the current interface. All structures should be placed in the “usb_device_descriptor.c” file.
Prototype:
typedef struct _usb_device_interface_struct
{
uint8_t alternateSetting;
usb_device_endpoint_list_t endpointList;
void* classSpecific;
} usb_device_interface_struct_t;
Description:
alternateSetting: The alternate value of this interface.
endpointList: endpoint list structure. See the usb_device_endpoint_list_t structure.
classSpecific: The class-specific structure pointer.
Prototype:
typedef struct _usb_device_endpoint_list
{
uint8_t count;
usb_device_endpoint_struct_t* endpoint;
} usb_device_endpoint_list_t;
Description:
count: Number of endpoints in the current interface.
endpoint: Endpoint information structure.
This is an example for the composite device MSD + CDC:
MSD:
usb_device_interface_struct_t g_mscDiskInterface[] =
{
{
0,
{
USB_MSC_DISK_ENDPOINT_COUNT,
g_mscDiskEndpoints,
},
},
};
Number “0” holds the alternate setting value of the MSD interface.
USB_MSC_DISK_ENDPOINT_COUNT is the endpoint number for MSD interface when the alternate setting is 0.
“g_mscDiskEndpoints” is the endpoint detailed information structure. See usb_device_endpoint_struct_t section for more information.
CDC:
For control interface:
/* Define interface for communication class */
usb_device_interface_struct_t g_cdcVcomCicInterface[] =
{
{
0,
{
USB_CDC_VCOM_CIC_ENDPOINT_COUNT,
g_cdcVcomCicEndpoints,
},
}
};
Number “0” holds the alternate setting value of the CDC control interface.
USB_CDC_VCOM_CIC_ENDPOINT_COUNT is the endpoint number for control interface when the alternate setting is 0.
“g_cdcVcomCicEndpoints" is the endpoint detailed information structure. See usb_device_endpoint_struct_t section for more information.
For data interface:
/* Define interface for data class */
usb_device_interface_struct_t g_cdcVcomDicInterface[] =
{
{
0,
{
USB_CDC_VCOM_DIC_ENDPOINT_COUNT,
g_cdcVcomDicEndpoints,
},
}
};
Number “0” holds the alternate setting value of the CDC data interface.
USB_CDC_VCOM_DIC_ENDPOINT_COUNT is the endpoint number for control interface when the alternate setting is 0.
“g_cdcVcomDicEndpoints” is the endpoint detailed information structure. See usb_device_endpoint_struct_t section for more information.
Parent topic:USB composite device structures