Compressed binary file internals#
This article describes the structure of the
zephyr.signed.bin file when image
compression is enabled. You do not need to know these details to use the
image compression subsystem, but they can be beneficial if you want to
use them for verification or custom integration purposes.
For an example, see the following structure of the file:

LZMA Header#
The Lempel-Ziv-Markov chain Algorithm (LZMA) header is crucial for files
compressed using the LZMA method. It contains metadata essential for
decompression. The lzma2_header encodes compression parameters using
two bytes.
Calculating compression parameters#
Compression parameters can be calculated, retrieved, or changed depending on your needs. For details, see the following sections.
Default values#
Compression parameters have the following default values:
dict_size: 131072pb: 2lc: 3lp: 1
Adjusting dictionary size#
You can calculate the dict_size using the following method:
unsigned int i = 0;
for (i = 0; i < 40; i++) {
if (raw_dict_size <= (((uint32_t)2 | ((i) & 1)) << ((i) / 2 + 11))) {
break;
}
}
dict_size = (uint8_t)i;
With this method, dict_size can have one of the following values:
Hex Value |
Size |
|---|---|
0x00 |
4096 |
0x01 |
6144 |
0x02 |
8192 |
0x03 |
12288 |
0x04 |
16384 |
0x05 |
24576 |
0x06 |
32768 |
0x07 |
49152 |
0x08 |
65536 |
0x09 |
98304 |
0x0a |
131072 |
0x0b |
196608 |
0x0c |
262144 |
0x0d |
393216 |
0x0e |
524288 |
0x0f |
786432 |
0x10 |
1048576 |
0x11 |
1572864 |
0x12 |
2097152 |
0x13 |
3145728 |
0x14 |
4194304 |
0x15 |
6291456 |
0x16 |
8388608 |
0x17 |
12582912 |
0x18 |
16777216 |
0x19 |
25165824 |
0x1a |
33554432 |
0x1b |
50331648 |
0x1c |
67108864 |
0x1d |
100663296 |
0x1e |
134217728 |
0x1f |
201326592 |
0x20 |
268435456 |
0x21 |
402653184 |
0x22 |
536870912 |
0x23 |
805306368 |
0x24 |
1073741824 |
0x25 |
1610612736 |
0x26 |
2147483648 |
0x27 |
3221225472 |
Calculating literal context, literal pos, and pos bits#
The second byte of the lzma2_header carries the following parameters:
lc, which specifies a number of literal context bitslp, which specifies a number of literal pos bitspb, which specifies a number of pos bitsThese parameters are encoded with the following formula:
pb_lp_lc = (uint8_t)((pb * 5 + lp) * 9 + lc);
To decode these values from the combined
pb_lp_lcbyte, run the following code:lc = pb_lp_lc % 9; pb_lp_lc /= 9; pb = pb_lp_lc / 5; lp = pb_lp_lc % 5;
Extracting LZMA stream from image#
To extract and decompress the LZMA stream from the image, follow these steps:
Determine the offset of the compressed stream by adding the
lzma2_headersize and the value stored underimage_header.ih_hdr_size. For the size of the compressed stream, seeimage_header.ih_img_size.If the compressed stream is isolated and stored in a file named
raw.lzma, you can perform decompression using the following commands:
Without an ARM thumb filter:
unlzma --lzma2 --format=raw --suffix=.lzma raw.lzma
With an ARM thumb filter:
unlzma --armthumb --lzma2 --format=raw --suffix=.lzma raw.lzma
Once the command is executed you will see a newly created file named
raw, which is identical to the
image before compression.
TLVs#
The following Type-Length-Values (TLVs) are used in the context of decompressed images:
DECOMP_SIZE (0x70): Specifies the size of the decompressed image.DECOMP_SHA (0x71): Contains the hash of the decompressed image.DECOMP_SIGNATURE (0x72): Holds the signature of either the hash or the entire image.
These TLVs are placed in the protected TLV section, ensuring they are included in the hashing and signature calculations during the verification process. The process for choosing the type of cryptographic signature and hash algorithm used for securing the image is the same, regardless of whether the image has undergone compression.
Sample#
For practical implementation, you can find a simple stand-alone
verification program under the following path
bootloader/mcuboot/samples/compression_test/independent_cmp.c
This program demonstrates how to independently verify the integrity and authenticity of a decompressed image using the specified TLVs.