Notes#
This section provides a list of notes to use EdgeFast Bluetooth stack
the follow configuration items related to resource needs more attention
CONFIG_BT_MAX_CONN The max connections that can be created.
CONFIG_BT_MAX_PAIRED The max supported paired devices.
CONFIG_BT_BUF_EVT_RX_COUNT The max received hci events and acl data packets at one time if the sys work queue task is blocked. One example is: when LE connection is created and HCI_LE_Enhanced_Connection_Complete is received, the sys work queue task is busy with processing the HCI_LE_Enhanced_Connection_Complete. If the received hci events exceed CONFIG_BT_BUF_EVT_RX_COUNT, it may leads potential issue, please increase value of the macro.
All the EdgeFast Bluetooth API should be called only after EdgeFast Bluetooth is initialized.
Don’t send HCI cmd from the sys work queue task or any stack’s callbacks.