Note#
The above steps are based on the a2dp_source example and help enable the peripheral_ht example on the m4 core. You can use the same steps for other examples and migrate them from an m7 project to an m4 project.
The above steps are based on the a2dp_source example and help enable the peripheral_ht example on the m4 core. You can use the same steps for other examples and migrate them from an m7 project to an m4 project.