Application programmers interface (API)#
This section describes the application programming interface (API) libraries of the SSRC module.
Type definitions#
This section describes the type definitions of the SSRC module.
Types for allocation of instance and scratch memory#
The instance memory is the memory that contains the state of one instance of the SSRC module. Multiple instances of the SSRC module can exist, each with it is own instance memory. S memory is the memory that is only used temporarily by the process function of the SSRC module. This memory can be used as scratch memory by any other function running in the same thread as the SSRC module. Different threads cannot share the scratch memories.
The application must allocate both the instance and the scratch memory. The SSRC module does not allocate memory.
There is a data type available for both the instance and the scratch memory, namely SSRC_Instance_t and SSRC_Scratch_t. The instance type is defined as structures of the correct size in the SSRC header file. Both the instance and the scratch memory must be 4 bytes aligned.
Parent topic:Type definitions
LVM_Fs_en#
Definition:
typedef enum
{
LVM_FS_8000 = 0,
LVM_FS_11025 = 1,
LVM_FS_12000 = 2,
LVM_FS_16000 = 3,
LVM_FS_22050 = 4,
LVM_FS_24000 = 5,
LVM_FS_32000 = 6,
LVM_FS_44100 = 7,
LVM_FS_48000 = 8
} LVM_Fs_en;
Description:
Used to pass the input and the output sample rate to the SSRC.
Parent topic:Type definitions
LVM_Format_en#
Definition:
typedef enum
{
LVM_STEREO = 0,
LVM_MONOINSTEREO = 1,
LVM_MONO = 2
} LVM_Format_en;
Description:
The LVM_Format_en enumerated type is used to set the value of the SSRC data format.
The SSRC supports input data in two formats Mono and Stereo. For an input buffer of NumSamples = N (meaning N sample pairs for Stereo and MonoInStereo or N samples for Mono), the format of data in the buffer is as listed in Table 1:
Sample Number |
Stereo |
MonoInStereo |
Mono |
|---|---|---|---|
0 |
Left(0) |
Mono(0) |
Mono(0) |
1 |
Right(0) |
Mono(0) |
Mono(1) |
2 |
Left(1) |
Mono(1) |
Mono(2) |
3 |
Right(1) |
Mono(1) |
Mono(3) |
4 |
Left(2) |
Mono(2) |
Mono(4) |
“ |
“ |
“ |
“ |
“ |
“ |
“ |
“ |
N-2 |
Left(N/2-1) |
Mono(N/2-1) |
Mono(N-2) |
N-1 |
Right(N/2-1) |
Mono(N/2-1) |
Mono(N-1) |
N |
Left(N/2) |
Mono(N/2) |
Not Used |
N+1 |
Right(N/2) |
Mono(N/2) |
Not Used |
N+2 |
Left(N/2+1) |
Mono(N/2+1) |
Not Used |
N+3 |
Right(N/2+1) |
Mono(N/2+1) |
Not Used |
“ |
“ |
“ |
Not Used |
“ |
“ |
“ |
Not Used |
2*N-2 |
Left(N-1) |
Mono(N-1) |
Not Used |
Parent topic:Type definitions
SSRC_Quality_en#
Definition:
typedef enum
{
SSRC_QUALITY_HIGH = 0,
SSRC_QUALITY_VERY_HIGH = 1,
SSRC_QUALITY_DUMMY = LVM_MAXENUM
} SSRC_Quality_en;
Description:
Used to select the quality level of the SSRC. For details, see Performance figures. Selecting the highest-quality level, comes with a cost in the SSRC processing requirements. Therefore, it should only be done for critical applications.
Parent topic:Type definitions
Instance parameters#
Definition:
typedef struct
{
SSRC_Quality_en Quality;
LVM_Fs_en SSRC_Fs_In;
LVM_Fs_en SSRC_Fs_Out;
LVM_Format_en SSRC_NrOfChannels;
short NrSamplesIn;
short NrSamplesOut;
} SSRC_Params_t;
Description:
Used to pass the SSRC instance parameters to the SSRC module. It is a structure that contains the members for input sample rate, output sample rate, the number of channels, and the number of samples on the input and output audio stream.
Parent topic:Type definitions
Nr of samples mode#
Definition:
typedef enum
{
SSRC_NR_SAMPLES_DEFAULT = 0,
SSRC_NR_SAMPLES_MIN = 1,
SSRC_NR_SAMPLES_DUMMY = LVM_MAXENUM
} SSRC_NR_SAMPLES_MODE_en;
Description:
The SSRC_NR_SAMPLES_MODE_en enumerated type specifies the two different modes that can be used to retrieve the number of samples using the SSRC_GetNrSamples function.
Parent topic:Type definitions
Function return status#
Definition:
typedef enum
{
SSRC_OK = 0,
SSRC_INVALID_FS = 1,
SSRC_INVALID_NR_CHANNELS = 2,
SSRC_NULL_POINTER = 3,
SSRC_WRONG_NR_SAMPLES = 4,
SSRC_ALLINGMENT_ERROR = 5,
SSRC_INVALID_MODE = 6,
SSRC_INVALID_VALUE = 7,
SSRC_ALLINGMENT_ERROR = 8,
LVXXX_RETURNSTATUS_DUMMY = LVM_MAXENUM
} SSRC_ReturnStatus_en;
Description:
The SSRC_ReturnStatus_en enumerated type specifies the different error codes returned by the API functions. For the exact meaning, see the individual function descriptions.
Parent topic:Type definitions
Parent topic:Application programmers interface (API)
Functions#
This section lists all the API functions of the SSRC module and explains their parameters.
SSRC_GetNrSamples#
Prototype:
SSRC_ReturnStatus_en SSRC_GetNrSamples
(SSRC_NR_SAMPLES_MODE_en Mode,
SSRC_Params_t* pSSRC_Params );
Description:
This function retrieves the number of samples or sample pairs for stereo used as an input and as an output of the SSRC module.
Name |
Type |
Description |
|---|---|---|
Mode |
SSRC_NR_SAMPLES_MODE_en |
There are two modes: |
pSSRC_Params |
SSRC_Params_t* |
Pointer to the instance parameters. The application fills in the values of the input sample rate, the output sample rate, and the number of channels. Based on this input, the |
Returns:
|
When the function call succeeds. |
|
When the requested input or output sampling rates are invalid. |
|
When the channel format is not equal to |
|
When |
|
When mode is not a valid setting. |
Note: The SSRC_GetNrSamples function returns the values from the following tables. Instead of calling the SSRC_GetNrSamples function, use the values from these tables directly.
Sample rate |
Nr of samples |
|---|---|
8000 |
320 |
11025 |
441 |
12000 |
480 |
16000 |
640 |
22050 |
882 |
24000 |
960 |
32000 |
1280 |
44100 |
1764 |
48000 |
1920 |
In/Out |
8000 |
11025 |
12000 |
16000 |
22050 |
24000 |
32000 |
44100 |
48000 |
|---|---|---|---|---|---|---|---|---|---|
8000 |
1 |
320 |
2 |
1 |
160 |
1 |
1 |
80 |
1 |
11025 |
441 |
1 |
147 |
441 |
1 |
147 |
441 |
1 |
147 |
12000 |
3 |
160 |
1 |
3 |
80 |
1 |
3 |
40 |
1 |
16000 |
2 |
640 |
4 |
1 |
320 |
2 |
1 |
160 |
1 |
22050 |
441 |
2 |
147 |
441 |
1 |
147 |
441 |
1 |
147 |
24000 |
3 |
320 |
2 |
3 |
160 |
1 |
3 |
80 |
1 |
32000 |
4 |
1280 |
8 |
2 |
640 |
4 |
1 |
320 |
2 |
44100 |
441 |
4 |
147 |
441 |
2 |
147 |
441 |
1 |
147 |
48000 |
6 |
640 |
4 |
3 |
320 |
2 |
3 |
160 |
1 |
Parent topic:Functions
SSRC_GetScratchSize#
Prototype:
SSRC_ReturnStatus_en SSRC_GetScratchSize
(SSRC_Params_t* pSSRC_Params,
LVM_INT32* pScratchSize );
Description:
This function retrieves the scratch size for a given conversion ratio and for given buffer sizes at the input and at the output.
Name |
Type |
Description |
|---|---|---|
|
|
Pointer to the instance parameters. All members should have a valid value. |
|
|
Pointer to the scratch size. The |
|
Returns:
|
When the function call succeeds. |
|
When the requested input or output sampling rates are invalid. |
|
When the channel format is not equal to |
|
When |
|
When the number of samples on the input or on the output are incorrect. |
Parent topic:Functions
SSRC_Init#
Prototype:
SSRC_ReturnStatus_en SSRC_Init
(SSRC_Instance_t* pSSRC_Instance,
SSRC_Scratch_t* pSSRC_Scratch,
SSRC_Params_t* pSSRC_Params,
LVM_INT16** ppInputInScratch,
LVM_INT16** ppOutputInScratch);
Description:
The SSRC_Init function initializes an instance of the SSRC module.
Name |
Type |
Description |
|---|---|---|
|
|
Pointer to the instance of the SSRC. This application must allocate the memory before calling the |
|
|
Pointer to the scratch memory. The pointer is saved inside the instance and is used by the |
|
|
Pointer to the instance parameters. |
|
|
The SSRC module can be called with the input samples located in scratch. This pointer points to a location that holds the pointer to the location in the scratch memory that can be used to store the input samples. For example, to save memory. |
|
|
The SSRC module can store the output samples in the scratch memory. This pointer points to a location that holds the pointer to the location in the scratch memory that can be used to store the output samples. For example, to save memory. |
Returns:
|
When the function call succeeds. |
|
When the requested input or output sampling rates are invalid. |
|
When the channel format is not equal to |
|
When |
|
When the number of samples on the input or on the output are incorrect. |
|
When the instance memory or the scratch memory is not 4 bytes aligned. |
Parent topic:Functions
SSRC_SetGains#
Prototype:
SSRC_ReturnStatus_en SSRC_SetGains
(SSRC_Instance_t* pSSRC_Instance,
LVM_Mode_en bHeadroomGainEnabled,
LVM_Mode_en bOutputGainEnabled,
LVM_INT16 OutputGain);
Description:
This function sets headroom gain and the post gain of the SSRC. The SSRC_SetGains function is an optional function that should be used only in rare cases. Preferably, use the default settings.
Name |
Type |
Description |
||||||||
|---|---|---|---|---|---|---|---|---|---|---|
|
|
Pointer to the instance of the SSRC. |
||||||||
|
|
Parameter to enable or disable the headroom gain of the SSRC. The default value is |
||||||||
|
|
Parameter to enable or disable the output gain. The default value is |
||||||||
|
|
The value of the output gain. The output gain is a linear gain value. 0x7FFF is equal to +6 dB and 0x0000 corresponds to -inf dB. By default, a 3 dB gain is applied (OutputGain = 23197), resulting in an overall gain of -3 dB (-6 dB headroom +3 dB output gain).
|
Returns:
|
When the function call succeeds |
|
When |
|
Wrong value used for the |
|
When |
Parent topic:Functions
SSRC_Process#
Prototype:
SSRC_ReturnStatus_en SSRC_Process
(SSRC_Instance_t* pSSRC_Instance,
LVM_INT16* pSSRC_AudioIn,
LVM_INT16* pSSRC_AudioOut);
Description:
Process function for the SSRC module. The function takes pointers as input and output audio buffers.
The sample format used for the input and output buffers is 16-bit little-endian. Stereo buffers are interleaved (L1, R1, L2, R2, and so on), mono buffers are deinterleaved (L1, L2, and so on).
Name |
Type |
Description |
|---|---|---|
|
|
Pointer to the instance of the SSRC. |
|
|
Pointer to the input samples. |
|
|
Pointer to the output samples. |
Returns:
|
When the function call succeeds. |
|
When one of |
Parent topic:Functions
SSRC_Process_D32#
Prototype:
SSRC_ReturnStatus_en SSRC_Process_D32
(SSRC_Instance_t* pSSRC_Instance,
LVM_INT32* pSSRC_AudioIn,
LVM_INT32* pSSRC_AudioOut);
Description:
Process function for the SSRC module. The function takes pointers as input and output audio buffers.
The sample format used for the input and output buffers is 32-bit little-endian. Stereo buffers are interleaved (L1, R1, L2, R2, and so on), mono buffers are deinterleaved (L1, L2, and so on).
Name |
Type |
Description |
|---|---|---|
|
|
Pointer to the instance of the SSRC. |
|
|
Pointer to the input samples. |
|
|
Pointer to the output samples. |
Returns:
|SSRC_OK|When the function call succeeds.|
|SSRC_NULL_POINTER|When one of pSSRC_Instance, pSSRC_AudioIn, or pSSRC_AudioOut is NULL.|
Parent topic:Functions
Parent topic:Application programmers interface (API)
Dynamic function usage#
This chapter explains how and when the SSRC functions are or can be used.
Define the number of samples to be used on input and output#
Call the function SSRC_GetNrSamples. Each integer multiple of the returned number of samples can be used.
Parent topic:Dynamic function usage
Allocate scratch memory#
To calculate the required size of the scratch memory, call the SSRC_GetScratchSize function. Allocate memory for the returned size.
Parent topic:Dynamic function usage
Initialize the SSRC instance#
Call the SSRC_Init function.
Parent topic:Dynamic function usage
Process samples#
The SSRC_Process function can now be called any number of times.
Parent topic:Dynamic function usage
Destroy the SSRC instance#
When the processing is completed, the allocated memory for the instance and the scratch can be freed.
Parent topic:Dynamic function usage
Parent topic:Application programmers interface (API)
Reentrancy#
None of the SSRC functions are re-entrant.
Parent topic:Application programmers interface (API)