canfd_interrupt_transfer_low_level#
Overview#
The canfd_interrupt_transfer_low_level example shows how to use FlexCAN driver in non-blocking interrupt way using low-level hardware APIs:
This example is similar to flexcan_interrupt_transfer but uses low-level hardware APIs instead of the transfer layer:
Does NOT use
flexcan_handle_torFLEXCAN_TransferCreateHandle()Does NOT use
FLEXCAN_TransferFDSendNonBlocking()/FLEXCAN_TransferFDReceiveNonBlocking()Uses direct hardware APIs:
FLEXCAN_WriteFDTxMb(),FLEXCAN_ReadFDRxMb(),FLEXCAN_GetMbStatusFlags(),FLEXCAN_ClearMbStatusFlags()ISR directly handles interrupts without transfer layer callback mechanism
In this example, two FlexCAN instances on a single board communicate with each other:
FlexCAN_RX is configured as receiver
FlexCAN_TX is configured as transmitter
When user presses any key in the terminal, FlexCAN_TX sends a CAN message to FlexCAN_RX
FlexCAN_RX receives the message and prints the content to the terminal
The data byte is incremented for each transmission
This design demonstrates one-way communication between two FlexCAN peripherals on the same board using low-level interrupt-driven APIs.