MCUXpresso SDK Documentation

Hardware requirements#

  • Mini USB cable

  • TWR-MC56F8400 board

  • Personal Computer

Board hardware common setting#

  1. Power setting:

    Connect J11 pin1 and pin2 Connect J6 pin1 and J7 pin2

  2. UART setting:

    Connect J8 pin3 and pin4 Connect J9 pin3 and pin4

  3. Onboard OSJTAG debugger setting:

    Connect J20 pin1 and pin2. Leave J17 open. Note: J17 is only used(connected) when firmware update for onboard debugger OSJTAG. Connect J21 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger OSJTAG. Note: when use external debugger(connected to J14), leave all J21 pins open

Board settings#

  • Supply external voltage(0~3.3V) to J503-3.

Prepare the Demo#

  1. Connect USB cable between the host PC and the JM60 USB(J18) port on the target board. It setups OSJTAG and COM port in PC device manager.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board with OSJTAG debug configuration.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo#

When the example runs successfully, the following message is displayed in the terminal:

ADC16 interrupt Example.
ADC16_DoAutoCalibration() Done.
ADC Full Range: 4096
Press any key to get user channel's ADC value ...
ADC Value: 1129
ADC Interrupt Count: 1
ADC Value: 1100
ADC Interrupt Count: 2
ADC Value: 1028
ADC Interrupt Count: 3
ADC Value: 1141
ADC Interrupt Count: 4
...