MCUXpresso SDK Documentation

Hardware requirements#

  • Mini USB cable

  • TWR-KM34Z75M board

  • Personal Computer

Board settings#

No special settings are required.

Prepare the Demo#

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo#

When the demo runs successfully, the following message is displayed in the terminal:

Starting channel No.0 ...
 Channel No.0 interrupt is occurred !
 Channel No.0 interrupt is occurred !
 Channel No.0 interrupt is occurred !
....................
....................
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
And you will find the LED RED is taking turns to shine.