Hardware requirements#
Mini USB cable
TWR-KM34Z75M board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo#
When the demo runs successfully, the following message is displayed in the terminal:
FLASH example Start
Flash Information:
Total Program Flash Size: xx KB, Hex: (xx)
Program Flash Sector Size: xx KB, hex: (xx)
...
Flash is xx
Erase a sector of flash
Successfully Erased Sector xx -> xx
Program a buffer to a sector of flash
Successfully Programmed and Verified Location xx -> xx
End of FLASH example