MCUXpresso SDK Documentation

Hardware requirements#

  • Mini USB cable

  • TWR-KM34Z75M board

  • Personal Computer

Board settings#

Connect J21 1-2 to use potentiometer

Prepare the Demo#

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

Roll the potentiometer(R21) to change the ADC value. When the demo runs successfully, the following message is displayed in the terminal:

ADC16 polling Example.
ADC16_DoAutoCalibration() Done.
Press any key to get user channel's ADC value ...
ADC Value: 1985
ADC Value: 1689
ADC Value: 1355
ADC Value: 1625
ADC Value: 1575
ADC Value: 1471