Hardware requirements#
Micro USB cable
TFT Proto 5” CAPACITIVE board HW REV 1.01 by Mikroelektronika. (Named as SSD1963 panel in project. Not necessary if use MIPI panel)
MIMXRT700-EVK
Personal Computer
RK055AHD091 MIPI panel (Not necessary if use other panel)
RK055IQH091 MIPI panel (Not necessary if use other panel)
RK055MHD091 MIPI panel (Not necessary if use other panel)
RM67162 smart MIPI panel (Not necessary if use other panel)
RaspberryPi Panel (Not necessary if use other panel)
ZC143AC72MIPI DBI panel (Not necessary if use other panel)
Board settings#
Use the external PMIC 5V power supply. Connect JP1 and JP3.
To use SSD1963 panel: Connect SSD1963 panel to J4. Make sure to connect JP7 2&3 to use 3.3v FLEXIO interface.
To use MIPI panel: Connect MIPI panel to J52.
To use Raspberry panel: Connect the panel to J8. Then connect the panel’s 5V pin to JP43-1, GND pin to JP43-2. Make sure the R75, R76, R79, R80 are connected.
To use the ZC143AC72MIPI panel: Connect J2 1&2.
Prepare the Demo#
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Steps to configure the panels#
The demo use MIPI RK055MHD091 panel by default. If Kconfig is used, select the panel in Kconfig “Panel Selection”. To use SSD1963 DBI panel, change the macro DEMO_PANEL to 4 in mcux_config.h. To use MIPI RK055AHD091 panel, change the macro DEMO_PANEL to 0 in mcux_config.h. To use MIPI RK055IQH091 panel, change the macro DEMO_PANEL to 1 in mcux_config.h. To use RM67162 MIPI smart DBI panel, change the macro DEMO_PANEL to 3 in mcux_config.h. To use MIPI RK055MHD091 panel, change the macro DEMO_PANEL to 2 in mcux_config.h(default). To use RaspberryPi, change the macro DEMO_PANEL to 5 in mcux_config.h. To use ZC143AC72MIPI DBI panel, change the macro DEMO_PANEL to 6 in mcux_config.h.
Frame buffer compression is supported for panels MIPI RK055MHD091 and MIPI RK055AHD091. In order to activate this support you have to select either MIPI RK055MHD091 or MIPI RK055AHD091 in Kconfig and set either DEMO_RK055MHD091_USE_XRGB8888 / DEMO_RK055AHD091_USE_XRGB8888 to 1 in mcux_config.h.
Running the demo#
When the example runs, you can see a polygon vector graphic with high render quality on a black buffer.