Hardware requirements#
Micro USB cable
MIMXRT700-EVK board
Personal Computer
SDIO card
Board settings#
JP65 1-2 connected.
Prepare the Demo#
Connect a micro USB cable between the PC host and the MCU-LINK USB port on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Note: Please insert the SDIO card into card slot(J47) after the debug console print “Please insert a card into board.”
Running the demo#
When the demo runs successfully, the log would be seen on the terminal like:
SDIO freertos example.
Card inserted.
Card init finished, ready to access.
Read function CIS, in direct way
CIS read successfully
Read function CIS, in extended way, non-block mode, non-word aligned size
Read function CIS, in extended way, block mode, non-word aligned size
The read content is consistent.
Input 'q' to quit card access task.
Input other char to access again