MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • MIMXRT700-EVK

  • Personal Computer

Board settings#

The MMC_SelectBusTiming in mmccard_init will fail, need to be commented out.

Prepare the Demo#

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J54) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo#

When the demo runs successfully, the log would be seen on the terminal like:

MMCCARD interrupt example.



Card user partition size xxxx bytes



Working condition:



  Voltage: xxxx



  Timing mode: xxxx



  Bus width: xxxx



  Freq : xxxx



Read/Write the card continuously until encounter error....



Write/read one data block......

Compare the read/write content......

The read/write content is consistent.

Write/read multiple data blocks......

Compare the read/write content......

The read/write content is consistent.

Erase data groups......



Input 'q' to quit read/write/erase process.

Input other char to read/write/erase data blocks again.