MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • MIMXRT700-EVK board

  • Personal Computer

Board settings#

Prepare the Demo#

  1. Connect a micro USB cable between the PC host and the USB port on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo#

Memory to memory copy demo - message from primary core side.
Memory to memory copy demo - message from ezhv core side.
Press any key to start the program.
DTCM_1 DST[0] = 0
DTCM_1 DST[1] = 1
DTCM_1 DST[2] = 2
DTCM_1 DST[3] = 3
DTCM_1 DST[4] = 4

DTCM_2 DST[0] = 0
DTCM_2 DST[1] = 1
DTCM_2 DST[2] = 2
DTCM_2 DST[3] = 3
DTCM_2 DST[4] = 4

SRAM DST[0] = 0
SRAM DST[1] = 1
SRAM DST[2] = 2
SRAM DST[3] = 3
SRAM DST[4] = 4

DTCM_1 DST[0] = 1
DTCM_1 DST[1] = 2
DTCM_1 DST[2] = 3
DTCM_1 DST[3] = 4
DTCM_1 DST[4] = 5
Memory to memory copy demo execute success.