MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • MIMXRT700-EVK board

  • Personal Computer

Board settings#

Prepare the Demo#

  1. Connect a micro USB cable between the PC host and the MCU-LINK on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo#

The log below shows the output of the hello world demo in the terminal window:

TRNG Peripheral Driver Example
Generate 10 random numbers: 
Random[0] = 0x201FEB53
Random[1] = 0x85A32C28
Random[2] = 0xDC66342C
Random[3] = 0xFD43ACFF
Random[4] = 0x1CD53C0
Random[5] = 0xB27EDBEB
Random[6] = 0x32AB81D5
Random[7] = 0x6AA5B70F
Random[8] = 0x81C41286
Random[9] = 0xC9620BD8

 Press any key to continue...